STM32H750 QSPI External Flash Programming Fails
- September 24, 2025
- 3 replies
- 390 views
I'm using an STM32H750XBH6 MCU with two external Flash(W25Q256 X2) chips connected via QSPI. I followed the guide (W25Q FLASH Memory || Part 10 || QSPI & External Loader on H750) to create a custom external loader (.stldr) using STM32CubeIDE, and I modified the loader to match my specific hardware setup.
However, programming fails and I receive the following error messages when using STM32 ST-LINK Utility:
16:07:41 : Timeout during flash programming
16:07:41 : Error occurred during erase operation!
16:07:41 : Unable to run On-Chip verification!
16:07:42 : Programmed memory Checksum: 0x00000000
16:07:48 : Cannot read external memory!
I've attached my loader source code for reference.
Could someone help me check if there are any mistakes or missing steps in my setup or configuration?
Thank you in advance!