Skip to main content
Associate II
August 30, 2025
Solved

STM32H750VBT6 CPU reset during microSD write, accompanied by Vcore (1.13V) drop

  • August 30, 2025
  • 2 replies
  • 396 views

Hello,

I am using STM32H750VBT6 to perform microSD card write operations. After a number of writes, the CPU sometimes resets during a write operation. At the same time, the Vcore (1.13V) rail shows a voltage drop. The issue is random, but the higher the write frequency, the faster it occurs. Below are details of my hardware, software, and test results.

 

1. Hardware design
The power supply module:

SandSwitch_0-1756560252796.png

  • The power supply is designed with 12V input, generating 3.8V, 3.3V, 1.8V, and 1.13V.

  • 3.3V powers the STM32 VDD pins, and 1.13V powers the VCAP pins.

  • Each VCAP pin is decoupled with a 0.1 µF capacitor in parallel with a 4.7 µF capacitor (located close, but not on the same plane due to vias).

The SD card interface:

SandSwitch_1-1756560276534.png

 

2. Software design

Initialization code generated by STM32CubeMX + HAL library:

 
void MX_SDMMC1_SD_Init(void)
{
 hsd1.Instance = SDMMC1;
 hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
 hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
 hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
 hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
 hsd1.Init.ClockDiv = 0;

 if (HAL_SD_Init(&hsd1) != HAL_OK) {
 Error_Handler();
 }
}

The write function (simplified):

int tfWriteBlock(uint32_t blockPosition, uint32_t numberOfBlocks, const uint8_t *buffer)
{
 for (uint32_t i = 0; i < numberOfBlocks; i++) {
 // Wait for card ready
 while (HAL_SD_GetCardState(&hsd1) != HAL_SD_CARD_TRANSFER) {
 osDelay(100);
 }

 // Write block
 if (HAL_SD_WriteBlocks_DMA(&hsd1, buffer, blockPosition + i, 1) != HAL_OK) {
 return ERR_FAIL;
 }

 // Wait for DMA completion
 if (xSemaphoreTake(semTFWrite, 100) != pdTRUE) {
 return ERR_TIMEOUT;
 }
 }
 return ERR_SUCCESS;
}

DMA complete callback:

void HAL_SD_TxCpltCallback(SD_HandleTypeDef *hsd)
{
 xSemaphoreGiveFromISR(semTFWrite, NULL);
}

In my testing process, I call the write function every 100 milliseconds, and each time I write 2 blocks.

 

3. Reset flags after abnormal reboot

I checked reset source flags using __HAL_RCC_GET_FLAG(). The results were:

RCC_FLAG_CPURST = 1
RCC_FLAG_D1RST = 1
RCC_FLAG_D2RST = 1

RCC_FLAG_PORRST = 0
RCC_FLAG_BORRST = 0
RCC_FLAG_PINRST = 0
RCC_FLAG_SFTRST = 0
RCC_FLAG_IWDG1RST = 0
RCC_FLAG_WWDG1RST = 0
RCC_FLAG_LPWR1RST = 0
RCC_FLAG_LPWR2RST = 0

 

4. microSD card testing

I tested three microSD cards:

  • Sandisk SDSQUNC-032G-ZN3MN → CPU reset occurs

  • Kingston SDCS3/64GB → No reset observed

  • Kingston SDCS2/32GB → No reset observed

So the issue seems to be card-dependent, happening only with the Sandisk card.

 

5. Power rail observation

Using an oscilloscope, I checked the power rails:

  • 3.8V and 3.3V → stable, no obvious ripple.

  • 1.13V (Vcore) → shows a significant voltage dip during the reset(waveform attached).

    SandSwitch_2-1756560559564.png

Additionally, I noticed that the problem only occurs when the external connector — which normally distributes 3.8V to other boards — is left unconnected. When the connector is attached (and the system is powering another board), the issue does not appear. Here‘s the connector interface:

SandSwitch_3-1756560739532.png

 

Question

Has anyone encountered a similar issue? Could this be related to Vcore stability, SDMMC peripheral behavior, or something in the power design? Any suggestions or experiences would be very helpful.

Best answer by SandSwitch

I finally find the root problem after trying a lot of changes in software and hardware.The sysclk frequency is too high.Using 143MHz instead of 286MHz solved the problem. Now sdmmc r&w never mistakes and mcu never reboots.

2 replies

AScha.3
Super User
August 30, 2025

Hi,

the problem is something in your hardware.

1. vcore from a smps - i would call it dangerous or at least: more problematic than using the internal LDO;

2. i use almost only Sandisk sd-cards, because they are the best/reliable , Kingston often "sick" after some time.

3. >the problem only occurs when the external connector .. is left unconnected. <

-> this obviously shows a problem, some imprecise connection , maybe ground loop , bad ground , etc.

Just strange is your "happening only with the Sandisk card" statement, because the card runs on 3v3 only;

so any internal resulting effect from different kind of cards could be afaik coming from different speed of card, 

that card and sdmmc , that the two make up each other, so maybe going to higher speed needs little more current, 

but this is only in the range of some mA .

I never seen a cpu core problem coming from a SD-card.

btw

My experience is from using H743 , H7A3, H733, H563 , with many different cards, 2GB...64GB, FAT and exFAT.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
August 31, 2025

Hi,

thank you for your suggestions.

I tried switching to the internal LDO regulator, but unfortunately I couldn’t get the MCU to start up properly in that mode.

Based on your reminder, I went back and checked my external Vcore supply design more carefully. I then realized that the decoupling capacitors on the VCAP pins were placed very far from the MCU pins — more than the distance of about 25 pin pitches, and connected through vias. This may have caused instability on the core supply. I am now correcting the placement of these capacitors (moving them closer to the VCAP pins) and will run further tests to see if this resolves the issue.

Best regards,
SandSwitch

SandSwitchAuthorBest answer
Associate II
December 14, 2025

I finally find the root problem after trying a lot of changes in software and hardware.The sysclk frequency is too high.Using 143MHz instead of 286MHz solved the problem. Now sdmmc r&w never mistakes and mcu never reboots.