STM32H7S7L8 MCE unable to write
Hello everyone,
I'm working on STM32H7S7L8 custom board with same architecture as the DK board ( for XSPIM)
The mcu and flash is working fine i can uplaud a boot/appli without issue (touch gfx + lwip work so the hardware is fine)
But working on the FW 1.3.0 I'm unable to make MCE work.
I followed step by step the MCE workshop : https://github.com/ST-TOMAS-Workshop/stm32h7s_workshop/blob/main/3_external_memory_encryption/external_memory_encryption.md
But when I build the extmem loader and try to uplaud the code I got :
Weird thing is that i already made MCE work on the DK board without issues but here it is not possible
Log output file: C:\Users\hdia\AppData\Local\Temp\STM32CubeProgrammer_a46772.log
ST-LINK SN : 002600493234510936303532
ST-LINK FW : V3J16M7B5S1
Board : STLINK-V3SET
Voltage : 3.31V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x485
Revision ID : Rev Y
Device name : STM32H7RSxx
Flash size : 64 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0xE3
Opening and parsing file: ST-LINK_GDB_server_a46772.srec
Memory Programming ...
File : ST-LINK_GDB_server_a46772.srec
Size : 1019.57 KB
Address : 0x90000000
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 133]
Erasing memory corresponding to segment 1:
Erasing external memory sectors [512 633]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:32.050
Verifying...
Error: Data mismatch found at address 0x90000001 (byte = 0x00 instead of 0x30)
Time elapsed during verifying operation: 00:00:01.517
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.300.202508131133\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.



Here the Cube MX settings that i used to make it (SBS also enabled in cube programmer / Cube MX ) and 192kb of DTCM setup
Do you have an Idea to make it work.
Thanks