Skip to main content
Associate III
December 16, 2025
Question

STM32H7S7L8H6: VBAT connection

  • December 16, 2025
  • 4 replies
  • 474 views

Hello Team,

 

Query related to VBAT. Please refer below capture and provide your feedback for VBAT. Diode D1 and other components are, ok? 

JK1234_0-1765442001969.png

Thanks & Regards,

Jignesh Karena

4 replies

TDK
Super User
December 16, 2025

Power dissipated by R218 if C56 is 0V is around 1.5 W which greatly exceeds the rated power value. Is C56 okay being charged at 500 mA? Can your 3.3V rail even supply that much excess current?

Generally want a much slower charge rate by increasing R218.

 

Diode reverse current seems a bit high. Probably better choices, but maybe it's good enough for your application.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JK1234Author
Associate III
December 16, 2025

Hello @TDK ,

Thanks for updates.

Can you please suggest best diode for this?

If we do not use R218 and connect direct connect it with VBAT pin via D1 diode than it is, ok? Refer below image.

JK1234_0-1765858210694.png

 

Thanks & Regards,

Jignesh Karena 

KDJEM.1
Technical Moderator
December 16, 2025

Hello @JK1234;

 

I recommend you to look at AN5935 application note Table 4. Power supply connection and Figure 3. Power supply component layout. The values of the two capacitors are 1 µF ceramic and 100 nF not 1F and 100 nF.

KDJEM1_0-1765873422078.png

KDJEM1_1-1765873534678.png

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JK1234Author
Associate III
December 16, 2025

Hello @KDJEM.1 ,

We want to use this solution for RTC. So, here 1F is super capacitor.

So, can you please provide some reference design for RTC using super capacitor?

 

Thanks & Regards,

Jignesh Karena

JK1234Author
Associate III
December 19, 2025

Hello Team,

Waiting for your feedback.

 

Thanks & Regards,

Jignesh Karena

KDJEM.1
Technical Moderator
December 19, 2025

Hello @JK1234 ;

 

Do you need more hardware information about how to retain the content of the RTC backup register?

Please look at 3.5 Battery charging domain.

KDJEM1_0-1766132378869.png

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
Super User
December 19, 2025

Do you have tools available to simulate this circuit? I suggest using those to see the effect of removing R218.

"If you feel a post has answered your question, please click ""Accept as Solution""."