Skip to main content
Explorer
June 12, 2025
Question

STM32L071CBT6 issue While recieving Input for GPIO pin

  • June 12, 2025
  • 1 reply
  • 234 views

 

STM32L071CBT6 GPIO PB15 Input Not Responding to 5V Signal from Buck Converter

Hello everyone,

I'm using the STM32L071CBT6 microcontroller and facing an issue with reading a digital input on GPIO pin PB15.

What I'm Trying to Do:

I’m using a buck converter with a 5V output to indicate the power status. The 5V output from the buck converter is connected to PB15, which is configured as a digital input on the STM32.

 

Setup:

  • Buck converter 5V output = GPIO PB15

  • Measured with multimeter: PB15 shows 5V when buck converter is ON

  • PB15 is configured in firmware as an input pin (floating or pull-down)

Problem:

Although PB15 is reading 5V on the pin when measured, the firmware logic that depends on PB15 being HIGH doesn't work.

 

What I’ve Checked:

  • The GPIO pin is correctly configured as input

  • Measured 5V directly at PB15

  • Tried enabling internal pull-down or external pull-down resistor

  • No response or logic change in the code when the 5V signal is applied

Why does PB15 show 5V physically (confirmed via multimeter) but the STM32L071 doesn't detect it as a logic HIGH in firmware?

1 reply

TDK
Super User
June 12, 2025

Set it as an output and drive it high and verify that (a) the voltage goes high and (b) the IDR register reflects this.

 

Related/duplicate? Just a coincidence you two asked the same uncommon question?

STM32L071CBT6 issue While recieving Input for GPIO... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."