STM32L433 Precise BusFault on GPIO access (BFAR = 0x48000000) despite enabling GPIO clock
I am working bare-metal on an STM32L433RCT6 (no HAL). I am seeing a precise data bus fault whenever I access a GPIO register.
Fault details from the debugger:
Fault type: Precise data bus fault
BFAR: 0x48000000
From RM0394, 0x48000000 is the GPIOA base address, so the fault occurs exactly on GPIO access.
The faulting instruction is a normal GPIO register read/write (e.g. ODR access). The GPIO struct layout and offsets are correct, and the compiler generates correct code.
I understand that on STM32, a precise bus fault on a valid peripheral address usually means the peripheral clock is disabled.
However, I explicitly enable the GPIO clock before accessing it:
*(volatile uint32_t*)0x4002104C |= (1 << 0); // RCC_AHB2ENR, GPIOAENAdditional context:
Custom register definitions for GPIO/RCC (not HAL)
Fault occurs before/at first GPIO access
Program resets and lands back in Reset_Handler
- BFAR(via Fault Analyzer) consistently reports 0x48000000
I will also attach the stm32l433xx.h, stm32l433xx_gpio_driver.h, stm32l433xx_gpio_driver.c code alongside the 001LedToggle.c file I am trying to execute.
stm32l433xx.h:
/*
* stm32l433xx.h
*
* Created on: Dec 29, 2025
* Author: Zaid
*/
#ifndef INC_STM32L433XX_H_
#define INC_STM32L433XX_H_
#include <stdint.h>
#define __vo volatile
#define FLASH_BASEADDR 0x08000000U
#define SRAM1_BASEADDR 0x20000000U
#define SRAM2_BASEADDR 0x10000000U
#define ROM_BASEADDR 0x1FFF0000U
#define SRAM1 SRAM1_BASEADDR
#define PERIPH_BASE 0x40000000U
#define APB1PERIPH_BASE PERIPH_BASE
#define APB2PERIPH_BASE 0x40010000U
#define AHB1PERIPH_BASE 0x40020000U
#define AHB2PERIPH_BASE 0x48000000U
/*Peripherals hanging on AHB2*/
#define GPIOA_BASEADDR (AHB2PERIPH_BASE + 0x0000)
#define GPIOB_BASEADDR (AHB2PERIPH_BASE + 0x0400)
#define GPIOC_BASEADDR (AHB2PERIPH_BASE + 0x0800)
#define GPIOD_BASEADDR (AHB2PERIPH_BASE + 0x0C00)
#define GPIOE_BASEADDR (AHB2PERIPH_BASE + 0x1000)
#define GPIOH_BASEADDR (AHB2PERIPH_BASE + 0x1C00)
#define RCC_BASEADDR (AHB1PERIPH_BASE + 0x1000)
/*Peripherals hanging on APB1*/
#define I2C1_BASEADDR (APB1PERIPH_BASE + 0x5400)
#define I2C2_BASEADDR (APB1PERIPH_BASE + 0x5800)
#define I2C3_BASEADDR (APB1PERIPH_BASE + 0x5C00)
#define SPI2_BASEADDR (APB1PERIPH_BASE + 0x3800)
#define SPI3_BASEADDR (APB1PERIPH_BASE + 0x3C00)
#define USART2_BASEADDR (APB1PERIPH_BASE + 0x4400)
#define USART3_BASEADDR (APB1PERIPH_BASE + 0x4800)
#define UART4_BASEADDR (APB1PERIPH_BASE + 0x4C00)
/*Peripherals hanging on APB2*/
#define USART1_BASEADDR (APB2PERIPH_BASE + 0x3800)
#define SPI1_BASEADDR (APB2PERIPH_BASE + 0x3000)
#define EXTI_BASEADDR (APB2PERIPH_BASE + 0x0400)
#define SYSCFG_BASEADDR (APB2PERIPH_BASE + 0x0000)
typedef struct
{
__vo uint32_t MODER; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t OTYPER; /*!<GPIO port output type register, Address offset: 0x04*/
__vo uint32_t OSPEEDR; /*!<GPIO port output speed register, Address offset: 0x08*/
__vo uint32_t PUPDR; /*!<GPIO port pull-up/pull-down register, Address offset: 0x0C*/
__vo uint32_t IDR; /*!<GPIO port input data register, Address offset: 0x10*/
__vo uint32_t ODR; /*!<GPIO port output data register, Address offset: 0x14*/
__vo uint32_t BSRR; /*!<GPIO port bit set/reset register, Address offset: 0x18*/
__vo uint32_t LCKR; /*!<GPIO port configuration lock register, Address offset: 0x1C*/
__vo uint32_t AFR[2]; /*!<AFR[0]: GPIO alternate function low register, AFR[1]: GPIO alternate function high register Address offset: 0x20-0x24*/
__vo uint32_t BRR; /*!<GPIO port bit reset register, Address offset: 0x28*/
}GPIO_RegDef_t;
typedef struct
{
__vo uint32_t CR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t ICSCR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CFGR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t PLLCFGR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t PLLSAI1CFGR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED0;
__vo uint32_t CIER; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CIFR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CICR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED1;
__vo uint32_t AHB1RSTR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB2RSTR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB3RSTR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED2;
__vo uint32_t APB1RSTR1; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB1RSTR2; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB2RSTR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED3;
__vo uint32_t AHB1ENR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB2ENR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB3ENR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED4;
__vo uint32_t APB1ENR1; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB1ENR2; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB2ENR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED5;
__vo uint32_t AHB1SMENR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB2SMENR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t AHB3SMENR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED6;
__vo uint32_t APB1SMENR1; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB1SMENR2; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t APB2SMENR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED7;
__vo uint32_t CCIPR; /*!<GPIO port mode register, Address offset: 0x00*/
uint32_t RESERVED8;
__vo uint32_t BDCR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CSR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CRRCR; /*!<GPIO port mode register, Address offset: 0x00*/
__vo uint32_t CCIPR2; /*!<GPIO port mode register, Address offset: 0x00*/
}RCC_RegDef_t;
#define GPIOA ((GPIO_RegDef_t*)GPIOA_BASEADDR)
#define GPIOB ((GPIO_RegDef_t*)GPIOB_BASEADDR)
#define GPIOC ((GPIO_RegDef_t*)GPIOC_BASEADDR)
#define GPIOD ((GPIO_RegDef_t*)GPIOD_BASEADDR)
#define GPIOE ((GPIO_RegDef_t*)GPIOE_BASEADDR)
#define GPIOH ((GPIO_RegDef_t*)GPIOH_BASEADDR)
#define RCC ((RCC_RegDef_t*)RCC_BASEADDR)
/*Enable Macros for GPIOx Peripherals*/
#define GPIOA_PCLK_EN() ( RCC->AHB2ENR |= (1 << 0))
//#define GPIOA_PCLK_EN() ( *(volatile uint32_t*)0x4002104C |= (1 << 0))
#define GPIOB_PCLK_EN() ( RCC->AHB2ENR |= (1 << 1))
#define GPIOC_PCLK_EN() ( RCC->AHB2ENR |= (1 << 2))
#define GPIOD_PCLK_EN() ( RCC->AHB2ENR |= (1 << 3))
#define GPIOE_PCLK_EN() ( RCC->AHB2ENR |= (1 << 4))
#define GPIOH_PCLK_EN() ( RCC->AHB2ENR |= (1 << 7))
/*Enable Macros for I2Cx Peripherals*/
#define I2C1_PCLK_EN() (RCC->APB1ENR1 |= (1<<21))
#define I2C2_PCLK_EN() (RCC->APB1ENR1 |= (1<<22))
#define I2C3_PCLK_EN() (RCC->APB1ENR1 |= (1<<23))
/*Enable Macros for SPIx Peripherals*/
#define SPI1_PCLK_EN() (RCC->APB2ENR |= (1<<12))
#define SPI2_PCLK_EN() (RCC->APB1ENR1 |= (1<<14))
#define SPI3_PCLK_EN() (RCC->APB1ENR1 |= (1<<15))
/*Enable Macros for USARTx Peripherals*/
#define USART1_PCLK_EN() (RCC->APB2ENR |= (1<<14))
#define USART2_PCLK_EN() (RCC->APB1ENR1 |= (1<<17))
#define USART3_PCLK_EN() (RCC->APB1ENR1 |= (1<<18))
/*Enable Macros for UARTx Peripherals*/
#define UART4_PCLK_EN() (RCC->APB1ENR1 |= (1<<19))
/*Enable Macros for SYSCFG Peripherals*/
#define SYSCFG_PCLK_EN() (RCC->APB2ENR |= (1<<0))
/*Disable Macros for GPIOx Peripherals*/
#define GPIOA_PCLK_DI() (RCC->AHB2ENR &= ~(1<<0))
#define GPIOB_PCLK_DI() (RCC->AHB2ENR &= ~(1<<1))
#define GPIOC_PCLK_DI() (RCC->AHB2ENR &= ~(1<<2))
#define GPIOD_PCLK_DI() (RCC->AHB2ENR &= ~(1<<3))
#define GPIOE_PCLK_DI() (RCC->AHB2ENR &= ~(1<<4))
#define GPIOH_PCLK_DI() (RCC->AHB2ENR &= ~(1<<5))
/*Disable Macros for I2Cx Peripherals*/
#define I2C1_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<21))
#define I2C2_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<22))
#define I2C3_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<23))
/*Disable Macros for SPIx Peripherals*/
#define SPI1_PCLK_DI() (RCC->APB2ENR &= ~(1<<12))
#define SPI2_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<14))
#define SPI3_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<15))
/*Disable Macros for USARTx Peripherals*/
#define USART1_PCLK_DI() (RCC->APB2ENR &= ~(1<<14))
#define USART2_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<17))
#define USART3_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<18))
/*Disable Macros for UARTx Peripherals*/
#define UART4_PCLK_DI() (RCC->APB1ENR1 &= ~(1<<19))
/*Enable Macros for SYSCFG Peripherals*/
#define SYSCFG_PCLK_DI() (RCC->APB2ENR &= ~(1<<0))
/*Macros to reset GPIOx peripherals*/
#define GPIOA_REG_RESET() do{RCC->AHB2RSTR |= (1<<0); RCC->AHB2RSTR &= ~(1<<0);}while(0)
#define GPIOB_REG_RESET() do{RCC->AHB2RSTR |= (1<<1); RCC->AHB2RSTR &= ~(1<<1);}while(0)
#define GPIOC_REG_RESET() do{RCC->AHB2RSTR |= (1<<2); RCC->AHB2RSTR &= ~(1<<2);}while(0)
#define GPIOD_REG_RESET() do{RCC->AHB2RSTR |= (1<<3); RCC->AHB2RSTR &= ~(1<<3);}while(0)
#define GPIOE_REG_RESET() do{RCC->AHB2RSTR |= (1<<4); RCC->AHB2RSTR &= ~(1<<4);}while(0)
#define GPIOH_REG_RESET() do{RCC->AHB2RSTR |= (1<<7); RCC->AHB2RSTR &= ~(1<<7);}while(0)
/*Generic Macros*/
#define ENABLE 1
#define DISABLE 0
#define SET ENABLE
#define RESET DISABLE
#define GPIO_PIN_SET SET
#define GPIO_PIN_RESET RESET
#include "stm32l433xx_gpio_driver.h"
#endif /* INC_STM32L433XX_H_ */
stm32l433xx_gpio_driver.h :
/*
* stm32l433xx_gpio_driver.h
*
* Created on: Jan 1, 2026
* Author: Zaid
*/
#ifndef INC_STM32L433XX_GPIO_DRIVER_H_
#define INC_STM32L433XX_GPIO_DRIVER_H_
#include "stm32l433xx.h"
typedef struct
{
uint8_t GPIO_PinNumber; /*!<possible values from @GPIO_PIN_NUMBER>*/
uint8_t GPIO_PinMode; /*!<possible values from @GPIO_PIN_MODE>*/
uint8_t GPIO_PinSpeed; /*!<possible values from @GPIO_PIN_SPEED>*/
uint8_t GPIO_PinPuPdControl; /*!<possible values from @GPIO_PIN_CONFIG>*/
uint8_t GPIO_PinOPType; /*!<possible values from @GPIO_OUTPUT_TYPE>*/
uint8_t GPIO_PinAltFunMode;
}GPIO_PinConfig_t;
typedef struct
{
GPIO_RegDef_t *pGPIOx; /*!<This holds the base address of the GPIO port to which the pin belongs>*/
GPIO_PinConfig_t GPIO_PinConfig;/*!<This holds the config settings of the GPIO port to which the pin belongs>*/
}GPIO_Handle_t;
/*
* @GPIO_PIN_NUMBER
* GPIO pin number
*/
#define GPIO_PIN_NO_0 0
#define GPIO_PIN_NO_1 1
#define GPIO_PIN_NO_2 2
#define GPIO_PIN_NO_3 3
#define GPIO_PIN_NO_4 4
#define GPIO_PIN_NO_5 5
#define GPIO_PIN_NO_6 6
#define GPIO_PIN_NO_7 7
#define GPIO_PIN_NO_8 8
#define GPIO_PIN_NO_9 9
#define GPIO_PIN_NO_10 10
#define GPIO_PIN_NO_11 11
#define GPIO_PIN_NO_12 12
#define GPIO_PIN_NO_13 13
#define GPIO_PIN_NO_14 14
#define GPIO_PIN_NO_15 15
/*
* @GPIO_PIN_MODE
* GPIO pin possible modes
*/
#define GPIO_MODE_IN 0
#define GPIO_MODE_OUT 1
#define GPIO_MODE_ALTFN 2
#define GPIO_MODE_ANALOG 3
#define GPIO_MODE_IT_FT 4
#define GPIO_MODE_IT_RT 5
#define GPIO_MODE_IT_RFT 6
/*
* @GPIO_OUTPUT_TYPE
* GPIO pin possible output types
*/
#define GPIO_OP_TYPE_PP 0
#define GPIO_OP_TYPE_OD 1
/*
* @GPIO_PIN_SPEED
* GPIO pin possible output speed
*/
#define GPIO_SPEED_LOW 0
#define GPIO_SPEED_MEDIUM 1
#define GPIO_SPEED_FAST 2
#define GPIO_SPEED_HIGH 3
/*
* @GPIO_PIN_CONFIG
* GPIO pin pull up AND pull down configuration macros
*/
#define GPIO_NO_PUPD 0
#define GPIO_PIN_PU 1
#define GPIO_PIN_PD 2
/*Peripheral Clock Control*/
void GPIO_PeriClockControl(GPIO_RegDef_t *pGPIOx, uint8_t EnorDi);
/*Init and De-Init*/
void GPIO_Init(GPIO_Handle_t *pGPIOHandle);
void GPIO_DeInit(GPIO_RegDef_t *pGPIOx);
/*Data read and write*/
uint8_t GPIO_ReadFromInputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber);
uint16_t GPIO_ReadFromInputPort(GPIO_RegDef_t *pGPIOx);
void GPIO_WriteToOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber, uint8_t Value);
void GPIO_WriteToOutputPort(GPIO_RegDef_t *pGPIOx, uint8_t Value);
void GPIO_ToggleOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber);
/*IRQ Configuration and ISR Handling*/
void GPIO_IRQConfig(uint8_t IRQNumber, uint8_t IRQPriority, uint8_t EnorDi);
void GPIO_IRQHandling(uint8_t PinNumber);
#endif /* INC_STM32L433XX_GPIO_DRIVER_H_ */
stm32l433xx_gpio_driver.c:
/*
* stm32l433xx_gpio_driver.c
*
* Created on: Jan 1, 2026
* Author: Zaid
*/
#include "stm32l433xx_gpio_driver.h"
/*
* *************************************************************
* @FN_it - GPIO_PeriClockControl
*
* @brief - Enables or disables peripheral clock for given GPIO port
*
* @PAram [in] - base address of gpio peripheral
* @PAram [in] - ENABLE or DISABLE macros
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
/*Peripheral Clock Control*/
void GPIO_PeriClockControl(GPIO_RegDef_t *pGPIOx, uint8_t EnorDi)
{
if(EnorDi == ENABLE)
{
if(pGPIOx == GPIOA)
{
//GPIOA_PCLK_EN();
*(volatile uint32_t*)0x4002104C |= (1 << 0);
}else if(pGPIOx == GPIOB)
{
GPIOB_PCLK_EN();
}else if(pGPIOx == GPIOC)
{
GPIOC_PCLK_EN();
}else if(pGPIOx == GPIOD)
{
GPIOD_PCLK_EN();
}else if(pGPIOx == GPIOE)
{
GPIOE_PCLK_EN();
}else if(pGPIOx == GPIOH)
{
GPIOH_PCLK_EN();
}
}
else
{
if(pGPIOx == GPIOA)
{
GPIOA_PCLK_DI();
}else if(pGPIOx == GPIOB)
{
GPIOB_PCLK_DI();
}else if(pGPIOx == GPIOC)
{
GPIOC_PCLK_DI();
}else if(pGPIOx == GPIOD)
{
GPIOD_PCLK_DI();
}else if(pGPIOx == GPIOE)
{
GPIOE_PCLK_DI();
}else if(pGPIOx == GPIOH)
{
GPIOH_PCLK_DI();
}
}
}
/*Init and De-Init*/
/*
* *************************************************************
* @FN_it - GPIO_Init
*
* @brief - Initializes GPIO port
*
* @PAram [in] - gpio config
* @PAram [in] -
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
void GPIO_Init(GPIO_Handle_t *pGPIOHandle)
{
uint32_t temp = 0; //temp. register
//1. Configure the mode of GPIO pin
if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode <= GPIO_MODE_ANALOG)
{
//non interrupt mode
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinMode << (2 * pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->MODER &= ~(0x3 << ( pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));//clearing
pGPIOHandle->pGPIOx->MODER |= temp;//setting
//temp = 0;
}else
{
// later (interrupt)
}
//2. Configure speed
temp = 0;
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinSpeed << (2 * pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->OSPEEDR &= ~(0x3 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);//clearing
pGPIOHandle->pGPIOx->OSPEEDR |= temp;//setting
temp = 0;
//3. Configure pupd settings
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinPuPdControl << (2 * pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->PUPDR &= ~(0x3 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);//clearing
pGPIOHandle->pGPIOx->PUPDR |= temp;//setting
temp = 0;
//4. Configure output type
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinOPType << (2 * pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->OTYPER &= ~(0x3 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);//clearing
pGPIOHandle->pGPIOx->OTYPER |= temp;//setting
temp = 0;
//5. Configure Alternate Functionality
if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode == GPIO_MODE_ALTFN)
{
//Configure the Alt Function registers
uint8_t temp1, temp2;
temp1 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber / 8;
temp2 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber % 8;
pGPIOHandle->pGPIOx->AFR[temp1] &= ~(0xF << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);//clearing
pGPIOHandle->pGPIOx->AFR[temp1] |= pGPIOHandle->GPIO_PinConfig.GPIO_PinAltFunMode << (4 * temp2);
}
}
/*
* *************************************************************
* @FN_it - GPIO_DeInit
*
* @brief - Deinitializes GPIO port
*
* @PAram [in] - gpio base address
* @PAram [in] -
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
void GPIO_DeInit(GPIO_RegDef_t *pGPIOx)
{
if(pGPIOx == GPIOA)
{
GPIOA_REG_RESET();
}else if(pGPIOx == GPIOB)
{
GPIOB_REG_RESET();
}else if(pGPIOx == GPIOC)
{
GPIOC_REG_RESET();
}else if(pGPIOx == GPIOD)
{
GPIOD_REG_RESET();
}else if(pGPIOx == GPIOE)
{
GPIOE_REG_RESET();
}else if(pGPIOx == GPIOH)
{
GPIOH_REG_RESET();
}
}
/*Data read and write*/
/*
* *************************************************************
* @FN_it - GPIO_ReadFromInputPin
*
* @brief - Reads from gpio pin
*
* @PAram [in] - gpio base address
* @PAram [in] - gpio pin number
* @PAram [in] -
*
* @return - 0 or 1
*
* @note - none
*
*/
uint8_t GPIO_ReadFromInputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber)
{
uint8_t value;
value = (uint8_t)((pGPIOx->IDR >> PinNumber) & 0x00000001);
return value;
}
/*
* *************************************************************
* @FN_it - GPIO_ReadFromInputPort
*
* @brief - Reads from gpio port
*
* @PAram [in] - gpio base address
* @PAram [in] -
* @PAram [in] -
*
* @return - value read at port
*
* @note - none
*
*/
uint16_t GPIO_ReadFromInputPort(GPIO_RegDef_t *pGPIOx)
{
uint16_t value;
value = (uint16_t)pGPIOx->IDR;
return value;
}
/*
* *************************************************************
* @FN_it - GPIO_WriteToOutputPin
*
* @brief - Writes to gpio pin
*
* @PAram [in] - gpio base address
* @PAram [in] - gpio pin number
* @PAram [in] - value to be written
*
* @return - none
*
* @note - none
*
*/
void GPIO_WriteToOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber, uint8_t Value)
{
if(Value == GPIO_PIN_SET )
{
//write 1 to output data register at the bit field corresponding to the pin number
pGPIOx->ODR |= (1 << PinNumber);
}else
{
pGPIOx->ODR &= ~(1 << PinNumber);
}
}
/*
* *************************************************************
* @FN_it - GPIO_WriteToOutputPort
*
* @brief - Writes to gpio port
*
* @PAram [in] - gpio base address
* @PAram [in] - value to be written
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
void GPIO_WriteToOutputPort(GPIO_RegDef_t *pGPIOx, uint8_t Value)
{
pGPIOx->ODR = Value;
}
/*
* *************************************************************
* @FN_it - GPIO_ToggleOutputPin
*
* @brief - Toggles gpio port
*
* @PAram [in] - gpio base address
* @PAram [in] - gpio pin number
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
void GPIO_ToggleOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber)
{
pGPIOx->ODR ^= (1 << PinNumber);
}
/*IRQ Configuration and ISR Handling*/
/*
* *************************************************************
* @FN_it - GPIO_IRQConfig
*
* @brief - Configures Interrupt
*
* @PAram [in] - address of gpio interrupt
* @PAram [in] - type of priority
* @PAram [in] - ENABLE or DISABLE macros
*
* @return - none
*
* @note - none
*
*/
void GPIO_IRQConfig(uint8_t IRQNumber, uint8_t IRQPriority, uint8_t EnorDi)
{
}
/*
* *************************************************************
* @FN_it - GPIO_IRQHandling
*
* @brief - Configures Interrupt for a pin
*
* @PAram [in] - gpio pin number
* @PAram [in] -
* @PAram [in] -
*
* @return - none
*
* @note - none
*
*/
void GPIO_IRQHandling(uint8_t PinNumber)
{
}
001LedToggle.c:
/*
* 001led_toggle.c
*
* Created on: Jan 7, 2026
* Author: Zaid
*/
#include "stm32l433xx.h"
void delay(void)
{
for(int i=0 ; i < 500000; i++);
}
int main(void)
{
GPIO_PeriClockControl(GPIOA,ENABLE);
GPIO_Handle_t GpioLed;
GpioLed.pGPIOx = GPIOA;
GpioLed.GPIO_PinConfig.GPIO_PinNumber = GPIO_PIN_NO_5;
GpioLed.GPIO_PinConfig.GPIO_PinMode = GPIO_MODE_OUT;
GpioLed.GPIO_PinConfig.GPIO_PinSpeed = GPIO_SPEED_FAST;
GpioLed.GPIO_PinConfig.GPIO_PinOPType = GPIO_OP_TYPE_PP;
GpioLed.GPIO_PinConfig.GPIO_PinPuPdControl = GPIO_NO_PUPD;
GPIO_Init(&GpioLed);
while(1)
{
GPIO_ToggleOutputPin(GPIOA, GPIO_PIN_NO_5);
delay();
}
return 0;
}