STM32U073: measure VBAT pin voltage when VDDA(3.0V) and VREF+(2.5V) are separated?
Hi everyone.
I'm using the STM32U073Mx / LQFP-80 pin.
While designing a schematic, I ran out of ports, so I'm curious to see if I can use the VDD (battery voltage) to VBAT pin trick to measure the battery voltage. I'm looking at the datasheet and reference manual(RM0503).
For reference, I'm using VREF+ as an Internal voltage reference mode to measure the temperature sensor (will use thermistor's power source), so I can no longer use the VREF+ pin as an input.
So, I'm trying to configure it as needed.
When measuring the thermistor temperature sensor, I use VREFBUFF(Internal voltage reference mode) to power the thermistor.
And for normal ADC operation, VREFBUFF(maybe Hold mode) is connected as the ADC reference voltage.
Anyway, I found the following sentence in the RM documentation, and I'd like to know its exact meaning.
[Temperature sensor, DAC output, VREFINT and VBAT internal channels
The temperature sensor is connected to channel ADC VIN[11].
The internal voltage reference VREFINT is connected to channel ADC VIN[12].
VBAT channel is connected to ADC VIN[13] channel.
The internal dac_out1 output voltage is connected to ADC VIN[19] channel.
When VREF+ is lower than VDDA, this channel is not converted.]
Is the conversion blocked(mean not converted) in hardware when VREF+ is lower than VDDA?
Or is the ADC functioning, but the converted value is unreliable?