STM32U375 current consumption at 80 Degrees temperature
Hello All,
I am current testing STM32U375RGT6Q at 80 degrees and I see that there is significant increase in the average current consumption at 80 degrees C. Average Current consumption increases from 290uA to 1mA.
Also note that
1) Pull up and Pull down are 1Mega
2) MCU is in sleep mode for 50 percent of the time.
3) Internal oscillator MSI is used at 3MHz
4) Flash memory is 1MB
5) SMPS mode is used to reduce the current consumption.
Is there a way out to reduce the current consumption at high temperature. I know that STM32L4 series are more stable over temperature but they dont suite the current budget of 300uA