Skip to main content
Associate
October 9, 2025
Solved

STM32U5G9NJ-DK1: OCTOSPI Auto-Polling Timeout in OctalPollingWEL() for Macronix Flash

  • October 9, 2025
  • 3 replies
  • 309 views

Hi,

I'm encountering an issue with OCTOSPI auto-polling on the STM32U5G9NJ-DK1 Discovery Kit while following the "Octo-SPI FLASH in Regular-command protocol example" from AN5050 (Rev 12, February 2025). Specifically, in the OctalPollingWEL() function, HAL_OSPI_AutoPolling() always times out while waiting for HAL_OSPI_FLAG_SM (Status Match) to set. It calls OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_SM, SET, tickstart, Timeout) and returns an error, triggering Error_Handler().

Link for Application Note:- https://www.st.com/resource/en/application_note/an5050-getting-started-with-octospi-hexadecaspi-and-xspi-interface-on-stm32-mcus-stmicroelectronics.pdf 

/* Octal polling Write enable latch function */
void OctalPollingWEL(void) {
 OSPI_AutoPollingTypeDef sConfig;
 OSPI_RegularCmdTypeDef sCommand;

 /* Initialize Indirect read mode for Software Polling to wait until WEL=1 */
 sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
 sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
 sCommand.Instruction = OCTAL_READ_STATUS_REG_CMD;
 sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
 sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_16_BITS;
 sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_ENABLE;
 sCommand.Address = 0x0;
 sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
 sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
 sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
 sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
 sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
 sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_ENABLE;
 sCommand.NbData = 2;
 sCommand.DummyCycles = DUMMY_CLOCK_CYCLES_READ_REG;
 sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
 sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;

 /* Set the mask to 0x02 to mask all Status REG bits except WEL */
 /* Set the match to 0x02 to check if the WEL bit is Set */
 sConfig.Match = WRITE_ENABLE_MATCH_VALUE;
 sConfig.Mask = WRITE_ENABLE_MASK_VALUE;
 sConfig.MatchMode = HAL_OSPI_MATCH_MODE_AND;
 sConfig.Interval = AUTO_POLLING_INTERVAL;
 sConfig.AutomaticStop = HAL_OSPI_AUTOMATIC_STOP_ENABLE;

 if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }

 /* Start Automatic-Polling mode to wait until the memory is ready WEL=1 */
 if (HAL_OSPI_AutoPolling(&hospi1, &sConfig, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }
}

/**
 * @brief Configure the OSPI Automatic Polling Mode in blocking mode.
 * @PAram hospi : OSPI handle
 * @PAram cfg : structure that contains the polling configuration information.
 * @PAram Timeout : Timeout duration
 * @note This function is used only in Automatic Polling Mode
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_OSPI_AutoPolling(OSPI_HandleTypeDef *hospi, OSPI_AutoPollingTypeDef *cfg, uint32_t Timeout)
{
 HAL_StatusTypeDef status;
 uint32_t tickstart = HAL_GetTick();
 uint32_t addr_reg = hospi->Instance->AR;
 uint32_t ir_reg = hospi->Instance->IR;
#ifdef USE_FULL_ASSERT
 uint32_t dlr_reg = hospi->Instance->DLR;
#endif /* USE_FULL_ASSERT */

 /* Check the parameters of the autopolling configuration structure */
 assert_param(IS_OSPI_MATCH_MODE(cfg->MatchMode));
 assert_param(IS_OSPI_AUTOMATIC_STOP(cfg->AutomaticStop));
 assert_param(IS_OSPI_INTERVAL(cfg->Interval));
 assert_param(IS_OSPI_STATUS_BYTES_SIZE(dlr_reg + 1U));

 /* Check the state */
 if ((hospi->State == HAL_OSPI_STATE_CMD_CFG) && (cfg->AutomaticStop == HAL_OSPI_AUTOMATIC_STOP_ENABLE))
 {
 /* Wait till busy flag is reset */
 status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_BUSY, RESET, tickstart, Timeout);

 if (status == HAL_OK)
 {
 /* Configure registers */
 WRITE_REG(hospi->Instance->PSMAR, cfg->Match);
 WRITE_REG(hospi->Instance->PSMKR, cfg->Mask);
 WRITE_REG(hospi->Instance->PIR, cfg->Interval);
 MODIFY_REG(hospi->Instance->CR, (OCTOSPI_CR_PMM | OCTOSPI_CR_APMS | OCTOSPI_CR_FMODE),
 (cfg->MatchMode | cfg->AutomaticStop | OSPI_FUNCTIONAL_MODE_AUTO_POLLING));

 /* Trig the transfer by re-writing address or instruction register */
 if (hospi->Init.MemoryType == HAL_OSPI_MEMTYPE_HYPERBUS)
 {
 WRITE_REG(hospi->Instance->AR, addr_reg);
 }
 else
 {
 if (READ_BIT(hospi->Instance->CCR, OCTOSPI_CCR_ADMODE) != HAL_OSPI_ADDRESS_NONE)
 {
 WRITE_REG(hospi->Instance->AR, addr_reg);
 }
 else
 {
 WRITE_REG(hospi->Instance->IR, ir_reg);
 }
 }

 /* Wait till status match flag is set to go back in idle state */
 status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_SM, SET, tickstart, Timeout);

 if (status == HAL_OK)
 {
 /* Clear status match flag */
 __HAL_OSPI_CLEAR_FLAG(hospi, HAL_OSPI_FLAG_SM);

 /* Update state */
 hospi->State = HAL_OSPI_STATE_READY;
 }
 }
 }
 else
 {
 status = HAL_ERROR;
 hospi->ErrorCode = HAL_OSPI_ERROR_INVALID_SEQUENCE;
 }

 /* Return function status */
 return status;
}

 
Regards,
Pavan

Best answer by KDJEM.1

Hello @PAV;

 

First of all thank you for updating post.

The configuration depends on the memory mode selected.

Below is the configuration for the OctalPollingWEL function in AN5050:

KDJEM1_1-1760085254913.png

Thank you.

Kaouthar

3 replies

KDJEM.1
Technical Moderator
October 9, 2025

Hello @PAV and welcome to the community;

 

Are you configuring the memory in DTR mode?

In your configuration, you have disabled DTR mode for the address 

sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE

I think it should be 

sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_ENABLE

Also, I recommend you to look at STM32CubeU5/Projects/STM32U5x9J-DK/Examples/OSPI/OSPI_NOR_MemoryMapped at main · STMicroelectronics/STM32CubeU5 · GitHub example may help you.

 

Thank you.

Kaouthar

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PAVAuthor
Associate
October 10, 2025

We have not made any changes to the code; it has been taken directly from the application note as a reference. However, we are facing an issue in the OctalPollingWEL() function, while the AutoPollingWIP() function works fine. For your reference, I am adding both the APIs below.

/* This function Configures Software polling to wait until WEL=1 */
void OctalPollingWEL(void) {
 OSPI_AutoPollingTypeDef sConfig;
 OSPI_RegularCmdTypeDef sCommand;

 /* Initialize Indirect read mode for Software Polling to wait until WEL=1 */
 sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
 sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
 sCommand.Instruction = OCTAL_READ_STATUS_REG_CMD;
 sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
 sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_16_BITS;
 sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_ENABLE;
 sCommand.Address = 0x0;
 sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
 sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
 sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
 sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
 sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
 sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_ENABLE;
 sCommand.NbData = 2;
 sCommand.DummyCycles = DUMMY_CLOCK_CYCLES_READ_REG;
 sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
 sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;

 /* Set the mask to 0x02 to mask all Status REG bits except WEL */
 /* Set the match to 0x02 to check if the WEL bit is Set */
 sConfig.Match = WRITE_ENABLE_MATCH_VALUE;
 sConfig.Mask = WRITE_ENABLE_MASK_VALUE;
 sConfig.MatchMode = HAL_OSPI_MATCH_MODE_AND;
 sConfig.Interval = AUTO_POLLING_INTERVAL;
 sConfig.AutomaticStop = HAL_OSPI_AUTOMATIC_STOP_ENABLE;

 if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }

 /* Start Automatic-Polling mode to wait until the memory is ready WEL=1 */
 if (HAL_OSPI_AutoPolling(&hospi1, &sConfig, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }
}


/* This function Configures Software polling mode to wait the memory is
ready WIP=0 */
void OctalPollingWIP(void) {
 OSPI_RegularCmdTypeDef sCommand;
 OSPI_AutoPollingTypeDef sConfig;

 /* Initialize Automatic-Polling mode to wait until WIP=0 */
 sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
 sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
 sCommand.Instruction = OCTAL_READ_STATUS_REG_CMD;
 sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
 sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_16_BITS;
 sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_ENABLE;
 sCommand.Address = 0x0;
 sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
 sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
 sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_ENABLE;
 sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
 sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
 sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_ENABLE;
 sCommand.NbData = 2;
 sCommand.DummyCycles = DUMMY_CLOCK_CYCLES_READ_REG;
 sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
 sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;

 /* Set the mask to 0x01 to mask all Status REG bits except WIP */
 /* Set the match to 0x00 to check if the WIP bit is Reset */
 sConfig.Match = MEMORY_READY_MATCH_VALUE;
 sConfig.Mask = MEMORY_READY_MASK_VALUE;
 sConfig.MatchMode = HAL_OSPI_MATCH_MODE_AND;
 sConfig.Interval = AUTO_POLLING_INTERVAL;
 sConfig.AutomaticStop = HAL_OSPI_AUTOMATIC_STOP_ENABLE;

 if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }

 /* Start Automatic-Polling mode to wait until the memory is ready WIP=0 */
 if (HAL_OSPI_AutoPolling(&hospi1, &sConfig, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) !=
 HAL_OK) {
 Error_Handler();
 }
}


 

KDJEM.1
KDJEM.1Best answer
Technical Moderator
October 10, 2025

Hello @PAV;

 

First of all thank you for updating post.

The configuration depends on the memory mode selected.

Below is the configuration for the OctalPollingWEL function in AN5050:

KDJEM1_1-1760085254913.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
October 16, 2025

Hello @PAV ;

 

Any update about the issue? 

If your issue is solved, please click on "Accept as Solution" on the reply which solved your issue.

 

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.