Skip to main content
Associate
October 10, 2025
Question

Swapped an STM401 with an STM412 and having issues, JLCPCB incorrect model?

  • October 10, 2025
  • 3 replies
  • 222 views

As title really. Keyboard project i'm working on in QMK required a bit more RAM so upgraded from the STMf401 to an STM32F412xE. Flashed firmware onto it RGB animations and OLED work correctly but USB device not recognised by computer. STM32cubeprogrammer shows 1mb of flash memory so concerned if JLCPCB have swapped it out for another model which would potentially be incompatible or just striahgt upgraded to the xG wtihout mentioning anything? Anybody experienced anything similar?

3 replies

TDK
Super User
October 11, 2025

What is the full part numbers of the chip you're moving from and moving to?

The part numbers are written on the package. Should be easy to read the top of the chip to see if what you ordered is what you got.

"If you feel a post has answered your question, please click ""Accept as Solution""."
OlligaterAuthor
Associate
October 13, 2025

Sorry for the late reply! Its an STM32F412CEU6 and i'm moving from the STM32F401CCU6

Karl Yamashita
Principal
October 14, 2025

Maybe I'm misinterpreting but it sounds like you just took the same FW from the STM32F401 and programmed the STM32F412? Or did you start a new project, configured the Clock, ported your code over and build again?

 

As for the flash size difference, does STM32Cube Programmer show enough Device information between the CE and CG, or it is showing xx?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Tesla DeLorean
Guru
October 14, 2025

Show the chip and USB portion of the schematic. The MCU should support USB connectivity with right circuit and firmware. 

Do you have an external crystal for HSE?

Perhaps try connecting with USB when you have BOOT0 strapped high. This should initiate the system loader at power up, check AN2606 for chip level features and pins, and if it supports USB you might expect to see "STM32 Boot Device".

This might tell you if it's wired correctly. 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..