Associate III
November 12, 2025
Solved
TIM15 in Slave Mode, Gated Mode to count the time a signal is High
- November 12, 2025
- 1 reply
- 170 views
Hi,
I want to count the time that an incoming level signal is high for.
To achieve this I setup Timer 15 as a Gated Mode Slave, which has it's counter counting while the trigger input is high. The trigger input is the Filtered Timer 15 Channel 1. For some reason when I connect my signal to my input Timer. Nothing Happens. The signal on the IO Pin TIM 15 CH1 is a 2V square Wave.
My own software seems correct. I then moved to Hal to see if I can achieve it.
I've tried to use HAL to achieve this without any luck here is my HAL software.
Uploaded is the main and IOC file
I am working on the STM32G071
Thanks