Skip to main content
waclawek.jan
Super User
January 20, 2026
Solved

'U5 SBus-via-DCACHE1 connectivity

  • January 20, 2026
  • 2 replies
  • 223 views

Is this connection real?

waclawekjan_0-1768924913136.png

I don't think so. DCACHE implementation subchapter says:

The DCACHE1 is placed on Cortex®-M33 S-AHB bus, and caches only the external RAM
memory region (OCTOSPI, HSPI, and FMC), in the address range [0x6000 0000:0xAFFF
FFFF] of the memory map.
Indeed, by placing a bus matrix demultiplexing node in front of the DCACHE1, S-AHB bus
memory requests addressing SRAM region or peripherals region (respectively in ranges
[0x2000 0000:0x3FFF FFFF] and [0x4000 0000:0x5FFF FFFF]) are routed directly to the
main AHB bus matrix, and the DCACHE1 is bypassed.

whereas the GFXMMU slave port is at 0x2400'0000.

JW

Best answer by Bubbles

Hi @waclawek.jan,

well spotted. It's confirmed to be there by mistake. We'll fix this in next RM revision, probably in few weeks time.

BR,

J

2 replies

mƎALLEm
Technical Moderator
January 20, 2026

Hello @waclawek.jan ,

I do agree with you. I will escalate and get back to you.

It could be a connection related to the Flash (a connection just below) not to that slave port but I need to confirm.

Internal ticket number 225541 for follow-up.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Bubbles
BubblesBest answer
ST Employee
January 22, 2026

Hi @waclawek.jan,

well spotted. It's confirmed to be there by mistake. We'll fix this in next RM revision, probably in few weeks time.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.