Skip to main content
Associate III
August 29, 2025
Question

Unable to import project created on TouchGFX into CubeIDE

  • August 29, 2025
  • 1 reply
  • 276 views

Hi,

I am currently working with the STM32H745I-DISCO development board. Initially, I followed a reference tutorial to successfully implement a basic LED blinking application utilizing both cores—Cortex-M4 and Cortex-M7.
Subsequently, I created a GUI-based project using TouchGFX Designer, which I then imported into STM32CubeIDE. The project compiled without errors; however, during the debugging phase, I encountered the following issue:

Error in final launch sequence: Failed to execute MI command: load C:\\TouchGFXProjects\\MyApplication_4\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf

Error message from debugger back end: Error finishing flash operation Failed to execute MI command: load C:\\TouchGFXProjects\\MyApplication_4\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf

Error message from debugger back end: Error finishing flash operation Failed to execute MI command: load C:\\TouchGFXProjects\\MyApplication_4\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf

Error message from debugger back end:

Error finishing flash operation.

Error finishing flash operation.

 

Screenshot 2025-08-29 100808.png

 

 

Screenshot 2025-08-29 100903.png

 

Screenshot 2025-08-29 100919.png

 

I would appreciate assistance in identifying and resolving this debugging issue.

 

1 reply

Associate III
September 8, 2025

Hi,

I posted a query a while ago and haven't received any response yet.  Could someone please check and let me know if more details are needed?