Unable to read internal temperature on STM32U575ZI using registers
Hello, I'm trying read core temperature. I use NUCLEO-U575ZI-Q board. I wrote code:
RCC->AHB3ENR |= RCC_AHB3ENR_PWREN;
PWR->SVMCR |= PWR_SVMCR_ASV;
RCC->AHB2ENR1 |= RCC_AHB2ENR1_ADC12EN;
ADC12_COMMON->CCR |= ADC_CCR_VSENSEEN;
ADC1->CR &= ~ADC_CR_DEEPPWD;
ADC1->CR |= ADC_CR_ADVREGEN;
while(!(ADC1->ISR & ADC_ISR_LDORDY));
ADC1->CR |= ADC_CR_ADCAL;
while (ADC1->CR & ADC_CR_ADCAL);
ADC1->CR |= ADC_CR_ADEN;
while (!(ADC1->ISR & ADC_ISR_ADRDY));
ADC1->DIFSEL = 0;
ADC1->PCSEL = ADC_PCSEL_PCSEL_19; // preselection
ADC1->SQR1 = (19 << ADC_SQR1_SQ1_Pos);
ADC1->SMPR2 |= (7 << ADC_SMPR2_SMP19_Pos); // max sample time
ADC1->CR |= ADC_CR_ADSTART;
while (!(ADC1->ISR & ADC_ISR_EOC));
uint16_t raw = ADC1->DR;
volatile float temperature_c =
(
(float)(raw - TS_CAL1) * (130.0f - 30.0f)
) / (float)(TS_CAL2 - TS_CAL1)
+ 30.0f;Unfortunately it doesn't work correctly. ADC1->DR returns always value 10499. It's looks like channel numer 19 wasn't connected to ADC. What do I incorrect?