Skip to main content
Dadigno
Associate III
October 14, 2025
Question

Unexpected Current Consumption in STOP2 Mode on STM32U595

  • October 14, 2025
  • 1 reply
  • 336 views

Hi everyone,

I’m facing an issue with power consumption in STOP2 mode on my custom board.
The board includes only the STM32U595 MCU, bypass and decoupling capacitors, and the inductor for the SMPS — nothing else is connected.

According to the datasheet, I expect a current consumption of around 4.65 µA in STOP2 mode (pag 214 Table 59, VDD = 3.3 V).

However, when I measure it with my STLINK Power Monitor, I get about ~10 µA with fast oscillations.

Dadigno_0-1760434701672.png

 

MX configuration:

  • All peripherals are disabled

  • SysClk = 16 MHz

  • All SRAM banks in Power-Down mode

  • Power saving mode enabled

  • SMPS enabled

  • Voltage scale = Range 4

  • All pins configured as analog input (via Project Manager → Code Generator)

Application code:

 HAL_DBGMCU_DisableDBGStopMode();
 HAL_Delay(5000);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 printf("Entering lowpower mode\r\n");
 HAL_Delay(500);
 HAL_SuspendTick();
 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
 // HAL_PWREx_EnterSHUTDOWNMode();
 }

Does anyone have an idea what could be causing this higher current consumption in STOP2 mode?
Any suggestions or insights would be greatly appreciated!

1 reply

Andrew Neil
Super User
October 14, 2025

@Dadigno wrote:

 on my custom board.


As it's a custom board, you need to show the schematics

How to write your question to maximize your chances to find a solution

 

Have you tried the ST examples on an ST board for reference?

Have you tried the ST examples on your custom board ?

AndrewNeil_0-1760435436236.png

https://www.st.com/resource/en/application_note/an5701-stm32cube-mcu-package-examples-for-stm32u5-series-stmicroelectronics.pdf#page=11

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Dadigno
DadignoAuthor
Associate III
October 14, 2025

@Andrew Neil 

Thank you for your quick reply.

No, I haven’t been able to test any examples on an ST board yet, but I used the official examples as a reference.

This is my current hardware setup. The board is actually more complex, but at the moment the only components populated are the ones shown in the photo — all other pins are floating.

 

Dadigno_0-1760436147800.png