Question
STM32F103 RS-485 only with HSI and HSI calibration?
Posted on September 08, 2015 at 09:21
It is
a good
idea to use
the
STM32F103
communicating over
RS485
(
38400bps
)
only
HSI
clock? STM32F103 will works in temperature -10 + 50C.I was looking at
the possibility of
user calibration
HSI
,
too
do not understand
. ST say.High-speed internal oscillator of 8 MHz, typically). At 25 °C, the HSI has an accuracy of ±1% typically, this is factory trimed.
The accuracy value of the RC frequency increases to the maximum value of -2% - +2,5
%
over temperature. -10 +105C. It can say, typically error is less than 80kHz. Maximum error is -160kHz +200kHzWhy is it
then
user triming RCC_CR register step 40kHz and user trimming range +- 640kHz?