Skip to main content
Associate III
June 27, 2025
Question

USB EMI Filter - USBUF01W6

  • June 27, 2025
  • 5 replies
  • 675 views

Hello Friends,

I am Using STM32F303 MCU for my FULL Speed USB  communication board. Used interrupt transfer.

Board is going to use in Noisy Industrial environment.

So , Planned to use Shielded USB cable with EMI Chokes ( Both Side ).

Cable Length is 1.8 Mtr.

I plan  to use ESD / EMI ICs on the board before the MCU like ....USBUF01W6  "OR"  USBLC6-2SC6.

Any Suggestion Which would be better out of two ?

 

Regards,

Bsuthar

5 replies

RobK1
Associate II
June 27, 2025

Seeing as how the USBUF01W6 offers EMI filtering in addition to ESD protection, that would seem to me the better choice in this case.

 

Whether or not it is good enough for your application is a different matter, though.

bsutharAuthor
Associate III
June 27, 2025

Hey Rob

Concern with USBUF01W6 is , Higher capacitance on D+ / D- line.  Also, it adds unwanted Series resistor I believe.

RobK1
Associate II
June 27, 2025

Just found out that STM have a USB Training. Its contents can be found here:

STM32_USB_training_Content.zip - Google Drive

It has a chapter on hardware design and, yes, it seems they do not want any series resistors in the data lines.

bsutharAuthor
Associate III
June 27, 2025

Hello Rob,

Thank you for sharing. It is Informative.

From the HW design Doc , They Mention to use USBLC6-4 instead USBLC6-2 for Self Powered.

I think we can use USBLC6-2 for Self Powered.

No specific reason I found for it.

With USB Type B connector , ID pin is not available. 

Technical Moderator
July 2, 2025

Hi @bsuthar 

You can check Table 13. ESD protection in AN4879 to find more about recommended ESD ICs.

I don't get your point about Type B connector and ID pin availability. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
bsutharAuthor
Associate III
July 2, 2025

Hello FBL,

Hardware design docs into STM32_USB_training_Content.zip - Google Drive

Suggests to use USBLC6-4SC6 instead USBLC6-2  for Self Powered Board , However , I could not retrieve the Reason...

May be because 4 Line Protection ( along with ID Pin )..

However , I used USBLC6-2 for D+/D- Line.

I have not used any separate ESD for VBUS line from the Host. I just connected it VBUS of USBLC6-2. ( See Schematic)

Await your valuable comments on that.

USBLCS6 - Connection Image.jpg

 

 

 

Technical Moderator
July 2, 2025

Hi @bsuthar 

We have two different implementations on different boards F303 eval board (MB1019) and F446 eval board  (MB1162)

FBL_0-1751472400031.png

FBL_1-1751472431803.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL