USB issues with STM32F103C8T6
Hello, I made a board with an STM32F103C8T6 which uses USB.
My issue is that when conecting USB (self powered or with external power) I get the following error on windows:
Windows has stopped this device because it has reported problems. (Code 43)
A request for the USB device descriptor failed.Things I checked:
- When no USB is connected, the D+ line is pulled to 3v3, but when connecting the USB it goes down to 2.8 with 0.5v being on the resistor.
- Checked continuity from USB header to A11 and A12 pins (when unpowered)
- Resolder pins to ensure propper contact (Except FL1, I checked that everything else is proppery soldered, but I guess continuity is a good proxy test)
- Changed MCU, USB header and FL1 for new ones in case they got damaged
- Firmware was tested with a bluepill and everything worked.
It's been a week with this issue, if someone know what could be happening or could give me tips to help diagnose this I'd appreciate it.
Here are the schematics for that part of the board:


And the layout: