Skip to main content
EPala.2
Associate III
June 10, 2025
Solved

Use PA0_C as GPIO on STM32H730IBK6Q

  • June 10, 2025
  • 2 replies
  • 708 views

Hi I am working on a project with STM32H730IBK6Q and STM32Cube IDE 1.16

I am trying to use PA0_C as a GPIO, but the GPIO function is not connecting properly. 

PA0 is used an ADC, not as a GPIO, so from how I understand muxing there should be no conflict. 

But when I try to use PA0_C it reads a static value, even after I confirm connectivity. 

How do I properly configure my project to use PA0_C as a gpio?

 

From the datasheet I got this cryptic instruction:

Analog switch between ports Pxy_C and Pxy PA0_C, PA1_C, PC2_C and PC3_C can be connected internally to PA0, PA1, PC2 and PC3, respectively (refer to SYSCFG_PMCR register in RM0468 reference manual). The switch is controlled by VDDSWITCH voltage level. It is defined through BOOSTVDDSEL bit of SYSCFG_PMCR. If the switch is closed the switch characteristics are given in the table below.

But nothing about what VDDSwitch is connected to physically or how to activate the pin properly in MX.

 

CubeMX doesn't throw any errors when I set up PA0_C as GPIO, it just generates code that doesn't work. 

Please advise, thanks! This project is in a final stage of development and the lack of documentation on this issue has put us in a tight spot. 

Best answer by mƎALLEm

Hello,

"I am trying to use PA0_C as a GPIO, but the GPIO function is not connecting properly. 

PA0 is used an ADC, not as a GPIO, so from how I understand muxing there should be no conflict. "

If you are using ADC and GPIO output on PA0x, you need to use PA0_C for the ADC input and PA0 for the GPIO output not the inverse. with the analog switch OPEN.

Meanwhile, PA0_C can be used as GPIO if the corresponding switch Pxy_SO is closed. So PA0 and PA0_C are connected and the alternate functions available on PA0 will be also available for PA0_C.

You need just to ensure that the switch is closed:

HAL_SYSCFG_AnalogSwitchConfig(SYSCFG_SWITCH_PA0, SYSCFG_SWITCH_PA0_CLOSE);

mALLEm_0-1749562786788.png

See also this FAQ: Default State of STM32H7 switches connecting Pxy_C and Pxy pads

 

2 replies

EPala.2
EPala.2Author
Associate III
June 10, 2025

Sharing screenshots of PA0_C and PA0 configuration. Note that PA0_C does not work even if I deactivate the ADC function on PA0.

Screenshot 2025-06-09 at 8.47.06 PM.pngScreenshot 2025-06-09 at 8.47.14 PM.png

TDK
Super User
June 10, 2025

PA0_C cannot be used as a GPIO independently of PA0.

You cannot use PA0 as an ADC and PA0_C as a GPIO.

You can use PA0_C as an ADC pin and PA0 as a GPIO.

TDK_0-1749521032951.png

 

 

If you're having issues or think an IOC is generating bad code, please attach it here so someone can take a look.

"If you feel a post has answered your question, please click ""Accept as Solution""."
EPala.2
EPala.2Author
Associate III
June 10, 2025

If PA0_C cannot be used as a GPIO while PA0 is used as an ADC why does CubeMX allow me to configure it them such without throwing a warning? The documentation of this is completely unclear, I searched both the datasheet and manual thoroughly without finding an explanation. The fact that nothing warned of this will create major costs in our development cycle that would have been completely avoidable if the documentation or development tools had made proper note of how this functioned.

TDK
Super User
June 10, 2025

Sometimes software has bugs. The latest STM32CubeMX version doesn't allow you to do this. You're a few versions behind.

The Reference Manual seems consistent to me in explanation, especially Figure 77. Only thing PA0_C can do on its own (i.e. without the analog switch) is ADC. When the switch is closed, the two pins are tied--they are no longer independent.

"If you feel a post has answered your question, please click ""Accept as Solution""."