Question
Use pin as both SPI MISO and GPIO/EXTI input
I use external ADC (slave) with pins with dual function. And when SPI don't work , on MISO pin can check and "end of conversion". This is when SPI pin NSS is high.
So: can I activate pin first like SPI "alternative pin" (pin is input - MISO) and like GPIO input using pooling or like "EXTI line".
Best Regards