Skip to main content
Associate
November 16, 2025
Question

Using QSPI PSRAM with a STM32-H753 is that possible?

  • November 16, 2025
  • 1 reply
  • 243 views

Hello,

I am in the process of designing a product which is based on the STM32-H753 and requires P/SRAM.

However, I'm concerned the H753 might not support on PSRAM with QSPI, I need the PSRAM for write/read.

I haven't found any application notes or examples from ST showing connection QSPI PSRAM into the STM32  only for FMC or OCTOSPI Flash.

Has anyone successfully used QSPI PSRAM with STM32H7 ?

Are the specific requirements or limitation I should be aware of ?

(attached reference images for context):

dvir1092_0-1763279213620.pngdvir1092_1-1763279246874.png

 

1 reply

AScha.3
Super User
November 16, 2025

Hi,

The STM32H753 microcontroller features a Quad-SPI (QSPI) memory interface designed specifically for Single, Dual, or Quad-SPI flash memories. This interface supports up to 256 Mbytes of external flash memory and can operate in direct, polling, or memory-mapped modes. However, the official documentation does not mention support for PSRAM (Pseudo-Static RAM) or other non-flash memories via the QSPI interface. The QSPI is intended for flash memory only, and there is no indication that it can be used for PSRAM or RAM chips.

+

For connecting PSRAM to the STM32H753, the recommended interface is the Flexible Memory Controller (FMC). The FMC is designed to support static-memory mapped devices, including PSRAM, and can handle up to 4 memory banks. It offers features such as independent chip select and configuration for each bank, and supports 8-, 16-, and 32-bit data bus widths. This makes the FMC the appropriate choice for interfacing PSRAM with the STM32H753.

+

Maybe other idea: look at the H7S3 /7 series with xspi :

AScha3_0-1763281523184.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
dvir1092Author
Associate
November 16, 2025

I Can't understand you sorry, 

If I'm using QSPI for connecting PSRAM why the MCU cares about who connect to him? the MCU communicate with PSRAM on QSPI interface and that's all? I don't need it to be memory mapped, just to store data .

this is the PSRAM

66-67WVS4M8ALL-BLL.pdf

AScha.3
Super User
November 16, 2025

Ok, i see,could work, so read :  AN4760

https://www.st.com/resource/en/application_note/an4760-quadspi-interface-on-stm32-microcontrollers-and-microprocessors--stmicroelectronics.pdf

+

I would do a real test: if you have a nucleo board with H7xx , connect a small so8 adapter with short wires and test it,

with the issi PSRAM . Not much effort , but then you know it 100% .

"If you feel a post has answered your question, please click ""Accept as Solution""."