Skip to main content
Associate
August 13, 2025
Question

Vbat minimum on STM32N6

  • August 13, 2025
  • 1 reply
  • 247 views

I am designing the power system for an application using the STM32N645. In the datasheet for the STM32N6x5 minimum Vbat is defined as "TBD". In the STM32N6570-DK schematic the Vbat rail is set to 3.3V. If it can operate at 1.8V it would simplify the power architecture.

Screenshot 2025-08-13 at 5.31.19 PM.png

Does anyone have any experience with running it at 1.8V? Or is there a timeline for when this specification will be released?

Thanks!

-Bash

1 reply

KDJEM.1
Technical Moderator
August 15, 2025

Hello @bashReflex and welcome to the Community;

 

I will check the minimum VBAT value on STM32N6 internally. I will get back to you as soon as possible.

Internal ticket number: 215811 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.