Skip to main content
WrenchInTheWorks
Associate II
July 5, 2025
Solved

Wake-up form EXTI not working on STM32G0B1 custom board

  • July 5, 2025
  • 2 replies
  • 311 views

Hello,

I'm attempting to make my MCU shift between STOP and RUN mode using a button. When I press the button the CPU stops, however, upon pressing again it fails to start the CPU. I know this form the LED indicators.

The strange part is that when I place a debug point, or anything debug related, the CPU wakes and immediately and runs the ISR as if it were waiting for the stop mode to resume.

Is there some setting I need to enable to get the GPIOs to funtion in stop0? 

I have had a look at other forum posts and MX examples but have not seen anything, or I have missed it.

My ISR:

void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin) {
 if (GPIO_Pin == Button_Pin && powerDownState == 0)
 {
 	powerDownState = 1;

 	HAL_GPIO_WritePin(Green_LED_GPIO_Port,Green_LED_Pin, GPIO_PIN_RESET); // Enable pull-up on button

 HAL_SuspendTick();
 HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
 }
 else
 {
 	HAL_ResumeTick();

 powerDownState = 0;

 HAL_GPIO_WritePin(Green_LED_GPIO_Port, Green_LED_Pin, GPIO_PIN_SET);
 }
}

 

GPIO_Init:

void MX_GPIO_Init(void)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(Green_LED_GPIO_Port, Green_LED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(Button_Drive_GPIO_Port, Button_Drive_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : Green_LED_Pin */
 GPIO_InitStruct.Pin = Green_LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(Green_LED_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : Button_Pin */
 GPIO_InitStruct.Pin = Button_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(Button_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : Button_Drive_Pin */
 GPIO_InitStruct.Pin = Button_Drive_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(Button_Drive_GPIO_Port, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI2_3_IRQn, 3, 0);
 HAL_NVIC_EnableIRQ(EXTI2_3_IRQn);

}

Cheers,
Michael

 

Best answer by TDK

Don't enter stop mode within an interrupt. The interrupt can't pre-empt itself.

Set a flag and handle going to sleep within the main loop.

2 replies

TDK
TDKBest answer
Super User
July 5, 2025

Don't enter stop mode within an interrupt. The interrupt can't pre-empt itself.

Set a flag and handle going to sleep within the main loop.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MM..1
Chief III
July 5, 2025

Use STOP in ISR callback is possible only with good knowledge and prepare registers state ... As @TDK  write never doit this way...