What is the internal clock CK_INT for the STM32H7 timers?
Hey
I know this is an old question, but I got into the situation to wonder about this too. After some research through the mystical STM documentation and some educated guesses I compiled this document. It might prevent others from the pain to find information in the STM documentation.
STM32H7B0VBT6 Timer Clock Sources
| Timer | APB Bus | Base Clock Source | Timer Kernel Clock | Clock Register |
| TIM1 | APB2 | rcc_pclk2 | rcc_timy_ker_ck | RCC_APB2ENR |
| TIM8 | APB2 | rcc_pclk2 | rcc_timy_ker_ck | RCC_APB2ENR |
| TIM15 | APB2 | rcc_pclk2 | rcc_timy_ker_ck | RCC_APB2ENR |
| TIM16 | APB2 | rcc_pclk2 | rcc_timy_ker_ck | RCC_APB2ENR |
| TIM17 | APB2 | rcc_pclk2 | rcc_timy_ker_ck | RCC_APB2ENR |
| TIM2 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM3 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM4 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM5 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM6 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM7 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM12 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM13 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
| TIM14 | APB1 | rcc_pclk1 | rcc_timx_ker_ck | RCC_APB1LENR |
Timer Clock Calculation
The actual timer kernel clock frequency depends on the APB prescaler and TIMPRE bit setting:
For APB1 Timers (rcc_timx_ker_ck):
- If CDPPRE1 = 0xx (no division) and TIMPRE = 0: Timer clock = rcc_hclk1
- If CDPPRE1 = 100 (÷2) and TIMPRE = 0: Timer clock = rcc_hclk1
- If CDPPRE1 = 101-111 (÷4 to ÷16) and TIMPRE = 0: Timer clock = 2 × rcc_pclk1
- If CDPPRE1 = 0xx (no division) and TIMPRE = 1: Timer clock = rcc_hclk1
- If CDPPRE1 = 100 (÷2) and TIMPRE = 1: Timer clock = rcc_hclk1
- If CDPPRE1 = 101 (÷4) and TIMPRE = 1: Timer clock = rcc_hclk1
- If CDPPRE1 = 110-111 (÷8 to ÷16) and TIMPRE = 1: Timer clock = 2 × rcc_pclk1
For APB2 Timers (rcc_timy_ker_ck):
- If CDPPRE2 = 0xx (no division) and TIMPRE = 0: Timer clock = rcc_hclk1
- If CDPPRE2 = 100 (÷2) and TIMPRE = 0: Timer clock = rcc_hclk1/2
- If CDPPRE2 = 101-111 (÷4 to ÷16) and TIMPRE = 0: Timer clock = 2 × rcc_pclk2
- If CDPPRE2 = 0xx (no division) and TIMPRE = 1: Timer clock = rcc_hclk1
- If CDPPRE2 = 100 (÷2) and TIMPRE = 1: Timer clock = rcc_hclk1/2
- If CDPPRE2 = 101 (÷4) and TIMPRE = 1: Timer clock = rcc_hclk1/4
- If CDPPRE2 = 110-111 (÷8 to ÷16) and TIMPRE = 1: Timer clock = 2 × rcc_pclk2
Notes:
- TIMPRE bit is located in RCC_CFGR register (bit 15)
- CDPPRE1 and CDPPRE2 are located in RCC_CDCFGR2 register
- All timers can be individually enabled/disabled via their respective enable bits
- The timer kernel clock is what feeds the timer prescaler and counter logic