Skip to main content
Associate II
May 28, 2025
Question

After modify the tsv file, rootfs can not run normally

  • May 28, 2025
  • 1 reply
  • 228 views

Hello

I want to remove the vendorfs and userfs from the ev board, so I modified the tsv file just like this:

longfeili_00001_0-1748423650128.png

after program the system of ev board, it looks like the rootfs cannot start up because the linux cannot recognize the rootfs partition:

longfeili_00001_1-1748423781314.png

the uuid of rootfs-a partition used by linux is not correct, how to correct the uuid?

 

1 reply

Christophe Guibout
ST Employee
June 3, 2025

Hello @longfeili_00001,

 

The partuuid described in the kernel command must be aligned with the partuuid of the rootfs-a or rootfs-b partition.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.