Can't blink a LED on STM32MP157-DK2
I'm now trying to blink a LED on my STM32MP157-DK2 board.
I have managed to run and even modify the GPIO_EXTI example, but I'd like to do this from scratch.
1) I first created a project using CubeMX and wrote my code in the IDE.
It seems that I can't use the BSP_LED_*** instructions as the build gives compilation errors : why can't I build my code when using these instructions ? Do I miss an include ?
2) Then I tried to use the HAL_GPIO_*** instructions. This time, the build is successful, but the debug does not blink the LED.
I have seen in the manual UM2367 that the blue LED is connected to PD11, so I try this:
HAL_GPIO_TogglePin (GPIOD, GPIO_PIN_11);
HAL_Delay (100); /* Insert delay 100 ms */but it doesn't blink. What did I miss?
Thanks for your help.