Connecting and debuging STM32MP157F with M4 core
Hi.
I'm trying to develop some SW on the M4 core of STM32MP157FAD1 on custom board with custom Linux.
After 2 days of fighting I'm finally able to run the tty echo example on it.
But I still struggle with connection to the board.
- Why CubeIDE Debugger requires Serial port?
We have the SSH accessible through the USB ETH over IP, that should be enough. - The Debugger resolve wrongly IP of the board:
We have pppd interface in the Linux. The debugger wrongly detects it's IP as the debugger IP.
It results with this error:
I'm also getting this error in console, it looks like the script/commands are interpreted wrongly:
- I'm still not able to get the ST-Link to work. It always ends with this error:

Thank you
P.S.
For others who also struggle to get it to work, check your device tree, CubeMX doesn't generate proper mbox m4_rproc. Add to end of the dts to the user section this:
&m4_rproc {
mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>, <&ipcc 3>;
mbox-names = "vq0", "vq1", "shutdown", "detach";
};To have the trace0 interface, you must add define for build preprocessor __LOG_TRACE_IO_