Question
Error booting from EMMC
When trying to boot from emmc I get the following error ...
�NOTICE: CPU: STM32MP157DAB Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157DAB-INSTRUO-SOM
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using EMMC
INFO: Instance 2
INFO: Boot used partition fsbl1
ERROR: Boot interface 2 not supported
PANIC at PC : 0x2ffebe9d
Exception mode=0x00000016 at: 0x2ffebe9dI assume this is an error with my tf-a bootloader?
I compiled tf-a with the build flag STM32MP_EMMC=1. Are there any other modifications/variables to set when building the tf-a to enable it to boot from emmc?