Skip to main content
Visitor II
February 13, 2025
Question

[ERROR] Couldn't find any video driver

  • February 13, 2025
  • 0 replies
  • 670 views

Hello, I have a problem after cross-compiling retroarch from my PC to an STM32MP135 (ARM32), after launching my ./retroarch -v I see that it will look for a video driver named "ext"

 

 

root@stm32mp1:/home/emu# ./retroarch -v
[INFO] [Config]: Looking for config in: "/home/root/.config/retroarch/retroarch.cfg".
[WARN] [GameMode]: GameMode cannot be enabled on this system ("dlopen failed - libgamemode.so: cannot open shared object file: No such file or directory.") https://github.com/FeralInteractive/gamemode needs to be installed.
[WARN] [Config]: GameMode unsupported - disabling..
[INFO] RetroArch 1.20.0 (Git b0999db)
[INFO] === Build =======================================
[INFO] CPU Model Name: ARMv7 Processor rev 5 (v7l)

[INFO] Capabilities: NEON VFPV3 VFPV4
[INFO] Version: 1.20.0
[INFO] Git: b0999db
[INFO] Built: Feb 11 2025
[INFO] =================================================
[ERROR] Couldn't find any video driver named "ext"
[INFO] Available video drivers are:
[INFO] null
[WARN] Going to default to first video driver..
[INFO] [Input]: Found input driver: "linuxraw".
[INFO] [Environ]: SET_PIXEL_FORMAT: RGB565.
[INFO] [Core]: Version of libretro API: 1, Compiled against API: 1
[INFO] [Core]: Geometry: 320x240, Aspect: 1.333, FPS: 60.00, Sample rate: 48000.00 Hz.
[INFO] [Video]: Set video size to: 960x720.
[ERROR] Couldn't find any video driver named "ext"
[INFO] Available video drivers are:
[INFO] null
[WARN] Going to default to first video driver..
[INFO] [Video]: Graphics driver did not initialize an input driver. Attempting to pick a suitable driver.
[ERROR] [Video]: Cannot initialize input driver. Exiting ...
[ERROR] Fatal error received in: "video_driver_init_internal()"
[INFO] [Core]: Content ran for a total of: 00 hours, 00 minutes, 00 seconds.
[INFO] [Core]: Unloading core..
[INFO] [Core]: Unloading core symbols..

 

 
 
For the cross compilation I did :
cd RetroArch
./configure --prefix=/path/to/install
export CC=arm-linux-gnueabihf-gcc
make

 

 

Does anyone have a solution?