Error during image compilation for STM32MP1 - glmark2
Hello there,
I have been trying to compile the newest release 2.0.0, first with some extra packages and also without them, but at around 90% the compilation process fails with following error:
ERROR: Task (/home/paradox/Desktop/workspace/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-openembedded/meta-oe/recipes-benchmark/glmark2/glmark2_git.bb:do_configure) failed with exit code '1'I am running the newest Ubuntu 20.04 LTS, which is not under officially supported distributions, however I don't believe that it is the real cause of the problem.
EDIT: It seems like it was really the 20.04 Ubuntu being an issue. The package was successfully built on the older 18.04, so my updated question is, will there be support for the newest Ubuntu version 20.04 and if so, approximately when could we expect it to be available?