Failed pre launch debugging with STM32CubeIDE
I am trying to debug a basic project on a STM32MP257F-DK board, and am running into an issue. This is the text of the error I get every time I debug:
'Launching <project>_CM33 Debug' has encountered a problem.
Error in final launch sequence:
Failed pre launch
========================
Error in final launch sequence:
Failed pre launch
Failed pre launch
Firmware remoteproc load failed, please:
1. make sure that /lib/firmware on your target has space
2. make sure that /lib/firmware has write access
> you can open a Console View for this..
Building results in no errors. I have verified that there is space and write access for the location it mentions, and I can see that the .elf file for the project gets written there. I have also gone through all the steps here without an issue: https://wiki.st.com/stm32mpu/wiki/STM32MP25_Discovery_kits_-_Starter_Package. I can also ssh into it without a problem. I have tried it on both Windows 11 and Ubuntu 24.04.
A couple other people have brought up similar issues, but their solutions did not let me get past this error. I had tried the solutions here and here, but there was no difference (changing the remote connections settings no difference, and there is only one qualifier I can choose).
Is there anything else I can try to get past this error message?