FreeBSD Port for mp157C
Hello! Is it feasible to start FBSD kernel?
So far I stuck with following error (seems to be from tf-a):
Loading kernel...
/boot/kernel/kernel text=0x1b4 text=0x5ad698 text=0x17e3d0 data=0xa4860 data=0x0+0x20c000 0x4+0x88d70+0x4+0xea43b|
Loading configured modules...
can't find '/etc/hostid'
can't find '/boot/entropy'
Using DTB compiled into kernel.
Kernel entry at 0xc0400200...
Kernel args: (null)
metadata: filename:/boot/kernel/kernel, size=11874740 loadaddr=0xc0400000
ERROR: Illegal access to 0xffff0010:
ERROR: FAIL_ID = 0x4c0
ERROR: Non-Secure
ERROR: Privilege
ERROR: Read
PANIC at PC : 0x2ffc97b1
Exception mode=0x00000016 at: 0x2ffc97b1
I'm sure, that control passes to the kernel _start point.
Any clues?