GPIO Interrupt / EXTI setup in device tree
I have the following DTS file and I have not been able to get the GPIO external interrupt working correctly. I have read this document on interrupt overviews, and tried to enable the EXTI to have control of the GPIOB pin 12.
/dts-v1/;
#include "stm32mp157.dtsi"
#include "stm32mp15xa.dtsi"
#include "stm32mp15-pinctrl.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15xx-dkx.dtsi"
/ {
model = "STMicroelectronics STM32MP157A-DK1 Discovery Board";
compatible = "st,stm32mp157a-dk1", "st,stm32mp157";
chosen {
stdout-path = "serial0:115200n8";
};
button {
compatible = "test,button";
input-gpios = <&gpiob 12 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>; //Works with pull-up once the driver is loaded.
interrupts-extended = <&gpiob 12 IRQ_TYPE_EDGE_FALLING>;
interrupt-names = "qwerty";
status = "okay";
};
led {
extern-led {
compatible = "test,led";
gpios = <&gpiob 10 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "cpu";
};
};
};The problem I have is that for all my gpio_to_irq() calls, I get the following:
[ 64.996864] platformdev: loading out-of-tree module taints kernel.
[ 65.003005] mod_probe() function was called.
[ 65.006308] mod_probe got miscdev minor id: 125
[ 65.010898] gpio_to_irq(0) = 88
[ 65.015773] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 1 already requested.
[ 65.022853] gpio_to_irq(1) = -6
[ 65.025872] gpio_to_irq(2) = 89
[ 65.028910] gpio_to_irq(3) = 90
[ 65.032338] gpio_to_irq(4) = 91
[ 65.035218] gpio_to_irq(5) = 92
[ 65.038271] gpio_to_irq(6) = 93
[ 65.041395] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 7 already requested.
[ 65.049669] gpio_to_irq(7) = -6
[ 65.052846] gpio_to_irq(8) = 94
[ 65.055812] gpio_to_irq(9) = 95
[ 65.058943] gpio_to_irq(10) = 96
[ 65.062249] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 11 already requested.
[ 65.070436] gpio_to_irq(11) = -6
[ 65.073796] gpio_to_irq(12) = 97
[ 65.076859] gpio_to_irq(13) = 98
[ 65.080112] gpio_to_irq(14) = 99
[ 65.083319] gpio_to_irq(15) = 100
[ 65.086619] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 0 already requested.
[ 65.094764] gpio_to_irq(16) = -6
[ 65.098248] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 1 already requested.
[ 65.106281] gpio_to_irq(17) = -6
[ 65.109559] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 2 already requested.
[ 65.117624] gpio_to_irq(18) = -6
[ 65.120821] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 3 already requested.
[ 65.128995] gpio_to_irq(19) = -6
[ 65.132198] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 4 already requested.
[ 65.140258] gpio_to_irq(20) = -6
[ 65.143562] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 5 already requested.
[ 65.151648] gpio_to_irq(21) = -6
[ 65.154987] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 6 already requested.
[ 65.163127] gpio_to_irq(22) = -6
[ 65.166210] gpio_to_irq(23) = 78
[ 65.169463] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 8 already requested.
[ 65.177710] gpio_to_irq(24) = -6
[ 65.180905] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 9 already requested.
[ 65.189071] gpio_to_irq(25) = -6
[ 65.192273] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 10 already requested.
[ 65.200433] gpio_to_irq(26) = -6
[ 65.203808] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 11 already requested.
[ 65.212052] gpio_to_irq(27) = -6
[ 65.215234] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 12 already requested.
[ 65.223441] gpio_to_irq(28) = -6
[ 65.226725] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 13 already requested.
[ 65.235007] gpio_to_irq(29) = -6
[ 65.238204] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 14 already requested.
[ 65.246450] gpio_to_irq(30) = -6
[ 65.249632] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 15 already requested.
[ 65.258245] gpio_to_irq(31) = -6
[ 65.261203] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 0 already requested.
[ 65.269297] gpio_to_irq(32) = -6
[ 65.272615] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 1 already requested.
[ 65.280607] gpio_to_irq(33) = -6
[ 65.283951] stm32mp157-pinctrl soc:pin-controller@50002000: irq line 2 already requested.
[ 65.292116] gpio_to_irq(34) = -6When I perform the IRQ request for the EXTI pin 12 input, with the gpio_to_irq number, provided above (#97) I get the IRQ, but it is not firing, because I believe the EXTI controller is not properly listening to GPIOB pin 12.
I want to connect to the gpio 28 (GPIOB pin 12), but the interrupt has already been claimed by GPIOA pin 12. So how do I change the EXTI controller to follow what I have defined in the DTS file and listen for GPIOB 12 instead?
I have tried the following DTS edits:
interrupts-extended = <&exti 28 IRQ_TYPE_EDGE_FALLING>;
------
interrupts-extended = <&gpiob 12 IRQ_TYPE_EDGE_FALLING>;
------
interrupt-parent = <&gpiob>;
interrupts = <12 IRQ_TYPE_EDGE_FALLING>;
------
If someone can explain what my DTS file should read I would appreciate it.
EDIT: I have temporarily connected the input pushbutton to the GPIO A12 pin, and the linux interrupt is working as expected, so what is misconfigured such that the EXTI isn't connected to GPIO port B? I cannot use pin A12, and I would much prefer to understand how this peripheral is configured.