Help me understand why L9733 device does not work
I am not able to launch SPI activation outputs just using datasheet information. I have tried everything and the status outputs do not change. By making use of an oscilloscope, I have checked that the data bytes transmitted (0xAC01, that would entail an activation of OUT1) through MISO line are correctly sent. Moreover, we have changed SPI mode, frequency, mode of sending the bits…but nothing happens.
I am not able to switch on/off internal mosfets after command byte writing operation. I also read fault register and get 0x0000, which indicates that no fault is present. I do not know if it is a timing issue or something else. I have changed the MCU used to act as a master, but nothing got.
Thanks in advance!