Skip to main content
Associate II
June 6, 2025
Question

How to connect the terminal to the STM32MP257-EV1 on the host computer

  • June 6, 2025
  • 1 reply
  • 451 views

Hi ST,

    I have flash the Android images(st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter) on the STM32MP257-EV1.

faye_Lee_2-1749188603147.jpeg

 

When booting the board(power supply by 5V3A adapter), the leds light as this status,is the board working normally?

faye_Lee_4-1749188791322.png

 

When the board booted and CN15 usb connected with PC , I found the device manager show the "Android aosp on stm32mp257f-ev1".When CN21 usb connected with PC, device manager shows up nothing new at all

faye_Lee_1-1749188586959.jpeg

The board was booting normally?If it is the normal status, how can I connect the terminal to the STM32MP257-EV1 on the host computer? 

 

1 reply

PatrickF
Technical Moderator
June 6, 2025

Hi, @faye_Lee 

If terminal is available (I'm sure for OpenSTLinux on EV1, Android should be same I assume), it should be available in one of the two virtual COM ports which should appear on the PC when connected to the ST-Link USB CN21.

 

Some help regarding terminal here (shown when running OpenSTLinux): https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Execute_basic_commands 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
faye_LeeAuthor
Associate II
June 6, 2025

Hi PatrickF,

    When I first boot the board, there were two virtual COM ports  appeared on the PC when connected to the ST-Link USB CN21 (STM32MP257-EV1's defualt image is OpenSTLinux?). But the second time I booted the board, there were  no virtual COM port  appeared on the PC. And then I flash the Android image on it, and it has no virtual COM port too. I wonder if my STM32MP257-EV1 board has some issue? How can I verify my STM32MP257-EV1 board whether work in normally status or not? Should I flash the default OpenSTLinux image? How can I flash the default OpenSTLinux image.

PatrickF
Technical Moderator
June 6, 2025

Hi,

Board STLINK virtual COM ports are completely independent of flashed image (it could be seen as an external Serial<->USB converter, like it is for an external ST-LINKV3-SET). They work as soon the USB is connected and recognized correctly as a valid USB. 

Maybe check your USB cable (sometimes, there is USB charging cables without data lines).

 

Regards,

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here