How to Integrate Cortex-M4 firmware into linux distribution
Hi, i am trying to build linux image along with cortex-m4 firmware which developed using STM32CubeIDE,
so for that i have copied a Stm32CubeIDE project under folder DistributionPackage/openstlinux-5.10-dunfell-mp1-21-03-31/layers/sources/m4projects-stm32mp1/Projects/STM32MP157C-DK2/Examples/TIM/project/project1/STM32CubeIDE/
Added the project path in /DistributionPackage/openstlinux-5.10-dunfell-mp1-21-03-31/layers/meta-st/meta-st-stm32mp/recipes-extended/m4projects/ m4projects-stm32mp1.bb
iam getting error as
arm-none-eabi-gcc: error: /home/akshay/project/stm32/DistributionPackage/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/m4projects-stm32mp1/1.4.0-r0/build/STM32MP157C-DK2/Examples/TIM/Project/JCIProject1/out/Debug//home/akshay/project/stm32/DistributionPackage/openstlinux-5.10-dunfell-mp1-21-03-31/layers/sources/m4projects-stm32mp1/Projects/STM32MP157C-DK2/Examples/TIM/Project/Project1/STM32CubeIDE/Common.o: No such file or directory
FYI : The file structure of example projects is different form the STM32CubeIDE project