Skip to main content
Senior II
April 15, 2025
Question

how to use qt 6 for cross compilation of stm32mp1

  • April 15, 2025
  • 0 replies
  • 417 views

This info i have got through chatgpt is this true?                                                                                                           The STM32MP1 Distribution Package (OpenSTLinux) traditionally supports Qt 5.15.x, with Qt 5.15.13 being the latest version officially integrated into the ecosystem. This version is commonly used in development environments for STM32MP1 devices.​

For newer versions of Qt, such as Qt 6.x, STMicroelectronics has introduced the X-LINUX-QT Expansion Package. However, as of the latest updates, this expansion package is primarily designed for the STM32MP2 series and is not yet fully functional with the STM32MP1 series. Therefore, if you're working with STM32MP1 devices, the officially supported Qt version remains at 5.15.13

 

If you require Qt 6.x features on STM32MP1, it would involve manual integration and building of Qt 6.x, which can be complex and is not officially supported.