Skip to main content
Associate III
August 13, 2024
Question

How to view and modify the current CPU frequency of STM32MP157D

  • August 13, 2024
  • 2 replies
  • 1704 views

Does anyone know how to view and modify the current CPU frequency of STM32MP157D? I also cannot use the following command:

 

root@stm32mp1:/sys# cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 48.00
Features : half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5

processor : 1
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 48.00
Features : half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5

Hardware : STM32 (Device Tree Support)
Revision : 0000
Serial : 003C00403132510831323338
root@stm32mp1:/sys# cd /
root@stm32mp1:/# cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 48.00
Features : half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5

processor : 1
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 48.00
Features : half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5

Hardware : STM32 (Device Tree Support)
Revision : 0000
Serial : 003C00403132510831323338

There is only BogoMIPS: 48 above, I want to know what to do with the current clock frequency of the CPU?

 

2 replies

Erwan SZYMANSKI
Technical Moderator
August 15, 2024

Hello @zengyixiang ,
You can check the minimum, maximum and current CPU frequency in this folder :

Board $> cd /sys/devices/system/cpu/cpufreq/policy0/

You can check following parameters :

  • cpuinfo_cur_freq
  • cpuinfo_max_freq
  • cpuinfo_min_freq

In the same folder, you have the scaling_governor that will manage the frequency changes. You can look online the documentation, but I think you can change it from schedutil to performance for example.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
August 16, 2024

Hello, I have seen it, but it seems that my CPU frequency is limited to 800MHz, with both the maximum and minimum being 800MHz. I would like to lower the frequency. How can I modify the minimum CPU frequency.

# pwd
/sys/devices/system/cpu/cpufreq/policy0
# cat cpuinfo_max_freq
800000
# cat cpuinfo_min_freq
800000
# cat cpuinfo_cur_freq
800000
#

 

Erwan SZYMANSKI
Technical Moderator
August 16, 2024

Hello @zengyixiang ,
Is it a personal PCB design ? 

The different CPU frequency configuration are described in OP-TEE and Linux device trees, in OPP tables nodes (operating points). On the last SW revision (OpenSTLinux 5.1) it is in stm32mp151.dtsi .

You can see the following :

cpu0_opp_table: cpu0-opp-table {
		compatible = "operating-points-v2";
		opp-shared;

		opp-400000000 {
			opp-hz = /bits/ 64 <400000000>;
			opp-microvolt = <1200000>;
			opp-supported-hw = <0x2>;
			opp-suspend;
		};

		opp-650000000 {
			opp-hz = /bits/ 64 <650000000>;
			opp-microvolt = <1200000>;
			opp-supported-hw = <0x1>;
			st,opp-default;
		};

		opp-800000000 {
			opp-hz = /bits/ 64 <800000000>;
			opp-microvolt = <1350000>;
			opp-supported-hw = <0x2>;
			st,opp-default;
		};
	};

It seems strange that your minimum is 800 MHz as for your revision, the 2 default mode we provide is 650 / 800. Can you please check that you have these definitions too ?

You should also be able to see these nodes in Linux kernel device trees. Please check it too.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
August 19, 2024

是的,我自己设计了 PCB,我的电源管理使用“EA3059QDR”芯片而不是“STPMIC1APQR”。我将VDDCORE固定在1.35V:

	vddcore: regulator-vddcore {
 compatible = "regulator-fixed";
		regulator-name = "vddcore";
		regulator-min-microvolt = <1350000>;
		regulator-max-microvolt = <1350000>;
		regulator-always-on;
 regulator-boot-on;
	};
&cpu0_opp_table {
		opp-800000000 {
			opp-hz = /bits/ 64 <800000000>;
			opp-microvolt = <1350000>;
			opp-supported-hw = <0x2>;
		};
		opp-400000000 {
			opp-hz = /bits/ 64 <400000000>;
			opp-microvolt = <1200000>;
			opp-supported-hw = <0x2>;
			opp-suspend;
		};
};