Howto configure ethernet0 MAC to MAC (without PHY, STM32MP157F)
Hi!
I hope there is someone with a little experience in this topic. We are trying to get eth0 without a PHY running.
HW development decided to connect an ethernet switch (LAN9668) directly to the eth0
interface. MDIO and RGMII are connected.
We are trying to describe the device-tree using the "fixed-link" property:
ðernet0 {
status = "okay";
pinctrl-0 = <ðernet0_rgmii_pins_a ðernet0_pps_pins_a>;
pinctrl-1 = <ðernet0_rgmii_sleep_pins_a ðernet0_pps_sleep_pins_a>;
pinctrl-names = "default", "sleep";
phy-mode = "rgmii-id";
max-speed = <1000>;
//phy-handle = <&phy0>;
nvmem-cells = <ðernet_mac_address>;
nvmem-cell-names = "mac-address";
fixed-link {
speed = <1000>;
full-duplex;
};
};We removed:
mdio0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0: ethernet-phy@0 {
reg = <0>;
};
};
};But we are still not able to get the link up.
With "phy0" still in, we got:
[ 14.242023] stm32-dwmac 5800a000.ethernet eth0: validation of rgmii-id with support 0000000,00000000,00006280 and advertisement 00002
[ 14.256200] stm32-dwmac 5800a000.ethernet eth0: no phy at addr -1
[ 14.267388] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Cannot attach to PHY (error: -19)With "fixed-link" a DMA problem is shown:
root@stm32mp1-nexio:~# dmesg | grep dwmac
[ 3.058021] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 3.062928] stm32-dwmac 5800a000.ethernet: no reset control found
[ 3.069358] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 3.075900] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 3.080703] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 3.087981] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 3.095392] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 3.102286] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 3.108675] stm32-dwmac 5800a000.ethernet: TSO supported
[ 3.113881] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 3.121707] stm32-dwmac 5800a000.ethernet: device MAC address de:52:74:ca:1a:ec
[ 3.128988] stm32-dwmac 5800a000.ethernet: Enabled Flow TC (entries=2)
[ 3.135586] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 3.141473] stm32-dwmac 5800a000.ethernet: Using 32 bits DMA width
[ 15.060089] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 15.064879] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 15.073856] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failedStudying
https://wiki.st.com/stm32mpu/wiki/ETH_internal_peripheral
and
https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration
did not help.
Thanks in advance!
BTW we are still using STM32MP15-Ecosystem-v3.1.0.
Bye Gunther