Question
I try spi communication, I write code using bare metal for master side(my board), using HAL library for slave board(STM32F429). My problem is that I can't receive data on slave board from master side.
I try to spi communication between my board with STM32MP157AACx microprocessor and STM32F429 disco board. I write code using bare metal for master side(my board), using HAL library for slave board(STM32F429). My problem is that I can't receive data from master side. There is my sample code piece from master side below:
int enable = 1;
uint8_t data;
uint8_t someval = 0x40;
void spi_init(void)
{
RCC->MC_AHB4ENSETR |= (1 << 1); //GPIOB peripheral clocks enable
RCC->MC_AHB4ENSETR |= (1 << 8); //GPIOI peripheral clocks enable
RCC->MC_APB1ENSETR |= (1<<11); //spi2 peripheral clocks enable
GPIOI->MODER &= ~(1<<2);
GPIOI->MODER |= (1<<3); //PI1 Alternate function
GPIOI->PUPDR &= ~(1<<2);
GPIOI->PUPDR &= ~(1<<3); //PI1 no pull up no pull down
GPIOI->MODER &= ~(1<<4);
GPIOI->MODER |= (1<<5); //PI2 Alternate function
GPIOI->PUPDR &= ~(1<<4);
GPIOI->PUPDR &= ~(1<<5); //PI2 no pull up no pull down
GPIOI->MODER &= ~(1<<6);
GPIOI->MODER |= (1<<7); //PI3 Alternate function
GPIOI->PUPDR &= ~(1<<6);
GPIOI->PUPDR &= ~(1<<7); //PI3 no pull up no pull down
GPIOB->MODER &= ~(1<<18);
GPIOB->MODER |= (1<<19); //Pb9 Alternate function
GPIOB->PUPDR &= ~(1<<18);
GPIOB->PUPDR &= ~(1<<19); //Pb9 no pull up no pull down
GPIOB->IDR |= (1<<9); //Pb9 GPIOB_IDR
GPIOI->AFR[0] |= (1<<4); //PI1 ALTERNETE FUNCTION
GPIOI->AFR[0] &= ~(1<<5);
GPIOI->AFR[0] |= (1<<6);
GPIOI->AFR[0] &= ~(1<<7);
GPIOI->AFR[0] |= (1<<8); //PI2 ALTERNETE FUNCTION
GPIOI->AFR[0] &= ~(1<<9);
GPIOI->AFR[0] |= (1<<10);
GPIOI->AFR[0] &= ~(1<<11);
GPIOI->AFR[0] |= (1<<12); // //PI3 ALTERNETE FUNCTION
GPIOI->AFR[0] &= ~(1<<13);
GPIOI->AFR[0] |= (1<<14);
GPIOI->AFR[0] &= ~(1<<15);
GPIOB->AFR[1] |= (1<<4); //PB9 ALTERNETE FUNCTION
GPIOB->AFR[1] &= ~(1<<5);
GPIOB->AFR[1] |= (1<<6);
GPIOB->AFR[1] &= ~(1<<7);
SPI2->CR2 |= (1<<0); //TSIZE (1 byte transfer)
SPI2-> CFG1 |= (1<<0); //SPI Data Frame 8 bit
SPI2-> CFG1 |= (1<<1);
SPI2-> CFG1 |= (1<<2);
SPI2-> CFG1 &= ~(1<<3);
SPI2-> CFG1 &= ~(1<<4);
SPI2-> CFG1 |= (1<<28); //SPI Master clock/256
SPI2-> CFG1 |= (1<<29);
SPI2-> CFG1 |= (1<<30);
/****************/
SPI2-> CFG2 &= ~(1<<24); //CPHA: the first clock transition is the first data capture edge
SPI2-> CFG2 &= ~(1<<25); //CPOL: SCK signal is at 0 when idle
SPI2-> CFG2 |= (1<<22); //spi master
SPI2-> CFG2 &= ~(1<<23); //MSB First
SPI2-> CFG2 |= (1<<29); //SSOE
SPI2-> CFG2 |= (1<<30); //SSOM
SPI2-> CR1 |= (1<<12); //SSI
SPI2-> CFG2 |= (1<<26); //SSM Enable
/*SPI Motorola*/
SPI2-> CFG2 &= ~(1<<21);
SPI2-> CFG2 &= ~(1<<20);
SPI2-> CFG2 &= ~(1<<19);
//SPI Communication Mode: FULL DUPLEX
SPI2-> CFG2 &= ~(1<<17);
SPI2-> CFG2 &= ~(1<<18);
SPI2-> CR1 |= (1<<0); //SPI Enable
SPI2-> CR1 |= (1<<9); //MASTER TRANSFER START
}
void spi_tx(uint8_t data)
{
while(!((SPI2->SR >> 1) & 1));
*(uint8_t*)&SPI2->TXDR = data;
while(((SPI2->SR >> 12) & 1));
}
uint8_t spi_rx(void)
{
while(((SPI2->SR >> 12) & 1));
*(uint8_t*)&SPI2->RXDR = 0;
while(!((SPI2->SR >> 0) & 1));
return SPI2->RXDR;
}
void Delay_us(uint16_t us)
{
TIM2->CNT = 0;
while (TIM2->CNT < us);
}
void Delay_ms(uint16_t ms)
{
for(uint16_t i=0; i<ms; i++)
{
Delay_us (1000); //delay of 1ms
}
}
void TIM2_IRQHandler(void){
TIM2->SR &= ~TIM_SR_UIF;
counter++;
}
void delay(uint32_t time)
{
while(time--);
}
int main(int argc, char **argv)
{
SysClockConfig();
TIM2_Config();
spi_init();
Delay_ms(10000);
while(1)
{
if(enable)
{
spi_tx(someval);
Delay_ms(1000);
}
}
}- Note: PI1: SPI2_SCK, PI2:SPI2_MISO, PI3: SPI2_MOSI, PB9: SPI2_NSS