Skip to main content
mdhebling
Associate
September 21, 2022
Question

I would like to know if is, there any STM32 MCU capable of receiving a video signal via I2C and sending it to an SDI video chip to convert to SDI format?

  • September 21, 2022
  • 4 replies
  • 3780 views

I ask because I'm starting the project of a converter that receives the video signal via optical fiber and converts it to an SDI output.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
September 21, 2022

I2C ? That seems contrived..

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
mdhebling
mdheblingAuthor
Associate
September 22, 2022

Tesla DeLorean, It isn't contrived!

The fiber optical transceiver that is delivered for us has I2C communication protocol output.

My doubt doesn't about I2C protocol but how I can use the SMPTE protocol with STM32 MCU or MPU.

I wrote two posts with the same doubt only why I'm respect the diferences betwen famylies ST and too I'm a new member in this comunity...

Tesla DeLorean
Guru
September 22, 2022

"Serial digital interface (SDI) is a standard for digital video and audio transmission over coaxial or fiber optic cabling. Speeds currently range from 270 megabits per second (Mbps) up to 12 gigabits per second (Gbps) for the latest standard released in 2015."

So you see my problem here is about 3 orders of magnitude, the only use of I2C would be tangential, ie you monitor or direct the flow of the fire-hose, you're definitely not going to be able to drink from it, let alone act on it, or forward it.

I don't see any of the STM32 range being able to Input then Output at these rates, in fact I'd imagine most solutions would keep this in hardware domain with some kind of continuous flow thru model or pipeline.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
mdhebling
mdheblingAuthor
Associate
September 22, 2022

@Community member​ I believe that I not supplied, initially, sufficient information to you help me, please forgive me.

If you have any suggestion, please inform me.

Thanks

Peter BENSCH
Technical Moderator
September 22, 2022

The doubts of @Community member​ were certainly due to the fact that insufficient information was initially provided. When talking about fiber optic, one typically has data rates of several Gbit in mind. However, there are indeed fibre optic transceivers for I2C coupling.

Nevertheless, "video signal" and I2C don't really match, because I2C normally works with 400kHz, in Fast Mode also with 1MHz, the fibre optic transceivers I saw so far only with 350kHz. With such small frequencies you can't transmit video signals in a meaningful way, because that would be like squeezing 100 trucks side by side and parallel on a normal motorway.

What is the specification of your video signal?

Regards

/Peter

mdhebling
mdheblingAuthor
Associate
September 22, 2022

@Peter BENSCH​ thank you for answer my question.

Answer your question, the specification of my video signal is based on SMPTE 297 protocol.

Basically my converter will receive the video signal by optical fiber and convert to SDI video standard. The video signal that will be received is provenience at video camera professional with optical fiber output, but other equipment used in the studio works with the SDI video input/output.

I need to know if ST has any chip that I can use with the optical fiber transceiver preprogrammed with the SMPTE 297 protocol to do the video conversion.

I'm talking with the some suppliers of optical fiber transceiver to understand how to work the communication betwen optical transceiver and microcontroller.

Peter BENSCH
Technical Moderator
September 22, 2022

As far as I know, SMPTE 297 is not a protocol, but only defines fibre optics as a transport medium. Other SMPTE standards then define the data rate at which transmission takes place, e.g. SMPTE 424M with 2.97Gbps. In any case, this is about a factor of 300...3000 above what I2C can do. I also assume that you have confused something.

STMicroelectronics does not have a ready-made chip for converting such amounts of data in its portfolio.

Regards

/Peter

PatrickF
Technical Moderator
September 22, 2022

Hi @mdhebling​ ,

I could assume your optical transceiver may have a ethernet interface such as RGMII + an I2C for link control. This is probably supported with Linux with STM32MP15x device.

Then, as I understand the video source come from fiber optic, it is unclear what is the destination of your video stream, but depending on video overall pixel/rate, it is probably possible to display it on LTDC/DSI or to store it on Linux Filesystem (in a compressed format).

But anyway, the STM32MP15x has no HW accelerators for video, so most processing should fit in SW which mean do not expect HD video quality..

Maybe look at following wiki pages

https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview

https://wiki.st.com/stm32mpu/wiki/GStreamer_overview

https://wiki.st.com/stm32mpu/wiki/How_to_stream_camera_over_network

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here