Skip to main content
Associate II
November 6, 2025
Question

Issue running STM32DDRFW-UTIL

  • November 6, 2025
  • 1 reply
  • 224 views

Hi team, 

I am able to successfully use pre-build binary from this https://github.com/STMicroelectronics/STM32DDRFW-UTIL.git repo for DDR4 with stm32mp257f-evk . but the generated artifacts with stm32 header by manually compiling in stm32cubeide I am facing the issue, After flashing I am not able to enter any command in the serial monitor window. 
I followed the build procedure explained in the repo's README.md

Vijay_kumar_0-1762416665196.png

As you can see in attached image only this DDR> prompt line is printed in serial port but not accepting any input from user , when I try to enter some command it reinitialized stdin to the same DDR> prompt line.

Thank you in advance...!!
hoping for a quick reply.

 

1 reply

PatrickF
Technical Moderator
November 6, 2025

Hi,

maybe just a local echo issue.

Did you have set the DDR_INTERACTIVE ?

Did you try blindly typing 'help' to see if any output ?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate II
November 7, 2025

@PatrickF 
Thanks for the reply..
I have setted DDR_INTERACTIVE as per REAMME.md 

Vijay_kumar_0-1762506767479.png

If I am using serial_putchar() I can able to flush data to my promt line but If I am using printf statements i can't getting any terminal output , Its getting stuck there .


I have created my own _write() function , __io_putchar() and tried using __attribute__(( weak )) this function for multiple definitions to make my function as priority.
I am suspecting printf() is not flushing data and getting stuck there it self. Can you help on
this ?

Regards, 

Vijay

 

PatrickF
Technical Moderator
November 7, 2025

Hi,

code should compile without any modifications. Please clarify you used the default github code as first intent.

Did you ensure the specific aarch64 prerequisites has been made ?
https://github.com/STMicroelectronics/STM32DDRFW-UTIL?tab=readme-ov-file#222-add-local-aarch64-toolchain 

Did you tried to debug the code with CubeIDE ?
https://github.com/STMicroelectronics/STM32DDRFW-UTIL?tab=readme-ov-file#224-launch-project 


Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here