Issue Using CubeMX Generated Files on STM32MP135DF with Kirkstone Yocto
Hi all,
I’m working with the STM32MP135DF board and trying to use a fully custom stack including Machine/Device Tree, Kernel, U-Boot, TF-A, and OP-TEE.
Here’s my setup:
Poky / Yocto version: kirkstone-4.0.27
CubeMX version: openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11
Added CubeMX generated files under:
meta-st/meta-st-stm32-Addons/mx/
└── stm32mp135df-comtrol
├── kernel
│ ├── Makefile
│ └── stm32mp135f-stm32mp135df-comtrol-mx.dts
├── optee-os
│ ├── conf.mk
│ └── stm32mp135f-stm32mp135df-comtrol-mx.dts
├── tf-a
│ ├── stm32mp135f-stm32mp135df-comtrol-mx.dts
│ ├── stm32mp135f-stm32mp135df-comtrol-mx-fw-config.dts
│ └── stm32mp13-mx.dtsi
└── u-boot
├── Makefile
├── stm32mp135f-stm32mp135df-comtrol-mx.dts
└── stm32mp135f-stm32mp135df-comtrol-mx-u-boot.dtsi
Generated custom machine by copying stm32mp13-disco-mx.conf.sample.
Successfully built the image.
Problem:
When I try to flash using the STM32 flashing tool Using Usb, it gets stuck after the 0x03 partition.
I suspect this is due to version mismatch between CubeMX-generated files and my Yocto version.
Questions:
How can I change the Yocto version in CubeMX so it matches my kirkstone-4.0.27 setup?
Am I missing any additional steps when integrating CubeMX generated files into an existing Yocto project?
Are there any known compatibility issues with openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11 files on kirkstone?
Any guidance, best practices, or examples would be highly appreciated.
Thanks!
boot Log while flashing
NOTICE: CPU: STM32MP135F Rev.Y
NOTICE: Model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11
NOTICE: Board: MB1635 Var1.0 Rev.E-02
INFO: PMIC version = 0x21
INFO: Reset reason (0x35):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.1(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: handle USB : Suspend int
INFO: USB Suspend mode
INFO: handle USB : Reset
INFO: handle USB : Reset
INFO: phase ID :3, Manifestation 0 at c716c3de
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x30006000
INFO: Image id=1 loaded: 0x30006000 - 0x30006246
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x30006000
INFO: FCONF: Reading firmware configuration information for: mce_config
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde200000
INFO: Image id=4 loaded: 0xde200000 - 0xde20001c
INFO: OPTEE ep=0xde200000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde200000
INFO: Image id=8 loaded: 0xde200000 - 0xde2792f8
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0400000
INFO: Image id=2 loaded: 0xc0400000 - 0xc040e7c8
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0000000
INFO: Image id=5 loaded: 0xc0000000 - 0xc00e4594
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde200000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Non-secure external DT found
I/TC: Embedded DTB found
I/TC: OP-TEE version: 3.16.0-dev (gcc version 11.4.0 (GCC)) #1 Fri Jan 28 02:28:18 PM UTC 2022 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
E/TC:0 0 stm32_clk_parse_fdt_opp:1772 2 MAX opp in st,ck_mpu
E/TC:0 0 Panic at core/drivers/clk/clk-stm32mp13.c:1773 <stm32_clk_parse_fdt_opp>
E/TC:0 0 TEE load address @ 0xde200000
E/TC:0 0 Call stack:
E/TC:0 0 0xde203cb5
E/TC:0 0 0xde21bf01
E/TC:0 0 0xde217bed
E/TC:0 0 0xde217e57
E/TC:0 0 0xde21aad7
E/TC:0 0 0xde21b015
E/TC:0 0 0xde216d29
E/TC:0 0 0xde216de9
E/TC:0 0 0xde216e07
E/TC:0 0 0xde216e07
E/TC:0 0 0xde216f83
E/TC:0 0 0xde21cbc1
E/TC:0 0 0xde203af7
E/TC:0 0 0xde200198
Cube Programmer
Image Folder
├── arm-trusted-firmware
│ ├── debug
│ │ ├── debug-tf-a-stm32mp135f-stm32mp135df-comtrol-mx-sdcard.stm32
│ │ ├── debug-tf-a-stm32mp135f-stm32mp135df-comtrol-mx-uart.stm32
│ │ ├── debug-tf-a-stm32mp135f-stm32mp135df-comtrol-mx-usb.stm32
│ │ ├── tf-a-bl2-stm32mp13-sdcard.elf
│ │ ├── tf-a-bl2-stm32mp13-uart.elf
│ │ └── tf-a-bl2-stm32mp13-usb.elf
│ ├── fwconfig
│ │ └── stm32mp135f-stm32mp135df-comtrol-mx-fw-config-optee.dtb
│ ├── metadata.bin
│ ├── tf-a-stm32mp135f-stm32mp135df-comtrol-mx-sdcard.stm32
│ ├── tf-a-stm32mp135f-stm32mp135df-comtrol-mx-uart.stm32
│ └── tf-a-stm32mp135f-stm32mp135df-comtrol-mx-usb.stm32
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.ext4
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.manifest
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.tar.xz
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol.ext4 -> core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.ext4
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol.manifest -> core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.manifest
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol.tar.xz -> core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.tar.xz
├── core-image-minimal-openstlinux-weston-stm32mp135df-comtrol.testdata.json -> core-image-minimal-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── fip
│ └── fip-stm32mp135f-stm32mp135df-comtrol-mx-optee.bin
├── flashlayout_core-image-minimal
│ ├── deleteall
│ │ └── FlashLayout_cubemx_stm32mp135f-stm32mp135df-comtrol-mx-deleteall.tsv
│ ├── extensible
│ │ └── FlashLayout_sdcard_stm32mp135f-stm32mp135df-comtrol-mx-extensible.tsv
│ └── optee
│ └── FlashLayout_sdcard_stm32mp135f-stm32mp135df-comtrol-mx-optee.tsv
├── kernel
│ ├── config-5.15.145
│ ├── Image -> Image--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── Image--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── Image-stm32mp135df-comtrol.bin -> Image--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── modules--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.tgz
│ ├── modules-stm32mp135df-comtrol.tgz -> modules--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.tgz
│ ├── modules-stripped--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.tgz
│ ├── modules-stripped-stm32mp135df-comtrol.tgz -> modules-stripped--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.tgz
│ ├── stm32mp135f-stm32mp135df-comtrol-mx--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.dtb
│ ├── stm32mp135f-stm32mp135df-comtrol-mx.dtb -> stm32mp135f-stm32mp135df-comtrol-mx--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.dtb
│ ├── stm32mp135f-stm32mp135df-comtrol-mx-stm32mp135df-comtrol.dtb -> stm32mp135f-stm32mp135df-comtrol-mx--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.dtb
│ ├── uImage -> uImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── uImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── uImage-stm32mp135df-comtrol.bin -> uImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── vmlinux -> vmlinux--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── vmlinux--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── vmlinux-stm32mp135df-comtrol.bin -> vmlinux--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── zImage -> zImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ ├── zImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
│ └── zImage-stm32mp135df-comtrol.bin -> zImage--5.15.145-stm32mp-r2.2-r0.1-stm32mp135df-comtrol-20251023130245.bin
├── optee
│ ├── debug
│ │ └── tee-stm32mp135f-stm32mp135df-comtrol-mx.elf
│ ├── tee-header_v2-stm32mp135f-stm32mp135df-comtrol-mx.bin
│ ├── tee-pageable_v2-stm32mp135f-stm32mp135df-comtrol-mx.bin
│ └── tee-pager_v2-stm32mp135f-stm32mp135df-comtrol-mx.bin
├── scripts
│ └── create_sdcard_from_flashlayout.sh
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.ext4
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.manifest
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.tar.xz
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol.ext4 -> st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.ext4
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol.manifest -> st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.manifest
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol.tar.xz -> st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.bootfs.tar.xz
├── st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol.testdata.json -> st-image-bootfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.cpio.gz
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.manifest
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol.cpio.gz -> st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.cpio.gz
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol.manifest -> st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.rootfs.manifest
├── st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol.testdata.json -> st-image-resize-initrd-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.ext4
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.manifest
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.tar.xz
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol.ext4 -> st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.ext4
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol.manifest -> st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.manifest
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol.tar.xz -> st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.userfs.tar.xz
├── st-image-userfs-openstlinux-weston-stm32mp135df-comtrol.testdata.json -> st-image-userfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.ext4
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.manifest
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.tar.xz
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol.ext4 -> st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.ext4
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol.manifest -> st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.manifest
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol.tar.xz -> st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.vendorfs.tar.xz
├── st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol.testdata.json -> st-image-vendorfs-openstlinux-weston-stm32mp135df-comtrol-20251023130245.testdata.json
├── st-initrd-openstlinux-weston-stm32mp135df-comtrol
└── u-boot
├── debug
│ └── u-boot-stm32mp13.elf
├── u-boot-nodtb-stm32mp13.bin
└── u-boot-stm32mp135f-stm32mp135df-comtrol-mx.dtb
14 directories, 82 files
Machine.conf
#@TYPE: Machine
#@NAME: stm32mp13-disco-mx
#@DESCRIPTION: [STM32CubeMX-EXAMPLE] STM32MP135F-DK board ONLY with Optee boot and SDcard support
#@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python
###########################################################################
#
# Default machine configuration sections
#
###########################################################################
include conf/machine/include/st-machine-common-stm32mp.inc
include conf/machine/include/st-machine-providers-stm32mp.inc
# Define specific common machine name
MACHINEOVERRIDES .= ":stm32mpcommonmx:stm32mp13commonmx"
MACHINEOVERRIDES .= ":stm32mp1common:stm32mp13common"
# =========================================================================
# Chip architecture
# =========================================================================
DEFAULTTUNE = "cortexa7thf-neon-vfpv4"
include conf/machine/include/arm/armv7a/tune-cortexa7.inc
# =========================================================================
# boot scheme
# =========================================================================
BOOTSCHEME_LABELS ?= ""
# =========================================================================
# boot device
# =========================================================================
BOOTDEVICE_LABELS ?= ""
# =========================================================================
# Machine settings
# =========================================================================
STM32MP_DEVICETREE = "${CUBEMX_DTB}"
# =========================================================================
# Machine features (default for stm32mp1 like)
# =========================================================================
MACHINE_FEATURES += "splashscreen"
MACHINE_FEATURES += "watchdog"
MACHINE_FEATURES += "nosmp"
# =========================================================================
# Device Storage
# =========================================================================
# Enable the board device storage support with CUBEMX_DTB according to BOOTDEVICE_LABELS
DEVICE_BOARD_ENABLE:SDCARD += "${@bb.utils.contains('BOOTDEVICE_LABELS', 'sdcard', '${CUBEMX_DTB}', '', d)}"
# =========================================================================
# Flashlayout
# =========================================================================
# Set the FLASHLAYOUT_TYPE_LABELS to CUBEMX_DTB according to BOOTDEVICE_LABELS
FLASHLAYOUT_TYPE_LABELS:sdcard = "${@bb.utils.contains('BOOTDEVICE_LABELS', 'sdcard', '${CUBEMX_DTB}', '', d)}"
# Specific settings for 'extensible' and 'deleteall' configurations
FLASHLAYOUT_CONFIG_LABELS:deleteall = "cubemx"
FLASHLAYOUT_TYPE_LABELS:deleteall:cubemx = "${CUBEMX_DTB}"
FLASHLAYOUT_TYPE_LABELS:extensible = "${CUBEMX_DTB}"
# =========================================================================
# CubeMX extra config
# =========================================================================
ENABLE_CUBEMX_DTB ?= "1"
###########################################################################
#
# User machine customization sections
#
###########################################################################
# Boot Scheme
# =========================================================================
BOOTSCHEME_LABELS += "optee"
# Boot Device Choice
# =========================================================================
# Define the boot device supported
BOOTDEVICE_LABELS += "sdcard"
# Support Feature Choice
# =========================================================================
# Define the features to enable on board
MACHINE_FEATURES += "bluetooth"
MACHINE_FEATURES += "wifi"
MACHINE_FEATURES += "usbg0"
# Specific firmwares and kernel modules configuration
# =========================================================================
# Set the list of kernel module to be auto-loaded during boot
KERNEL_MODULE_AUTOLOAD += ""
# Set Bluetooth related package list needed when 'bluetooth' feature is enabled
# NOTE 'linux-firmware-bluetooth-bcm4343' firmware is specific to BT/WIFI
# combo used on DISCO boards"
BLUETOOTH_LIST += "linux-firmware-bluetooth-bcm4343"
# Set Wifi related package list needed when 'wifi' feature is enabled
# NOTE 'linux-firmware-bcm43430' firmware is specific to BT/WIFI combo used
# on DISCO boards
WIFI_LIST += "linux-firmware-bcm43430"
# CubeMX Project Config
# =========================================================================
# Assign CubeMX Board devicetree and project path name
CUBEMX_DTB = "stm32mp135f-stm32mp135df-comtrol-mx"
CUBEMX_PROJECT = "mx/stm32mp135df-comtrol"
# Indicate which STM32MP package are used: 'A', 'C', 'D' or 'F'
CUBEMX_SOC_PACKAGE = "F"
# Indicate the size of DDR available on BOARD: 512 or 1024 (size in MB unit)
CUBEMX_BOARD_DDR_SIZE = "512"
# Indicate if you like to disable the DVFS which are activated by default
CUBEMX_SOC_DVFS_OFF = "0"