"Kernel Panic" boot error message when loading touchscreen driver
Hello all.
In my stm32mp1 linux yocto machine I'm attempting to modify the touchscreen devicetree to manage the GOODIX GT911 touchscreen driver.
Before modify the devicetree is the following
+&i2c2 {
+ pinctrl-names = "default", "sleep";
+ pinctrl-0 = <&i2c2_pins_a>;
+ pinctrl-1 = <&i2c2_pins_sleep_a>;
+ i2c-scl-rising-time-ns = <185>;
+ i2c-scl-falling-time-ns = <20>;
+ status = "okay";
+ /delete-property/dmas;
+ /delete-property/dma-names;
+
+ polytouch: edt-ft5x06@38 {
+ compatible = "edt,edt-ft5x06";
+ reg = <0x38>;
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_edt_ft5x06>;
+ interrupt-parent = <&gpiob>;
+ interrupts = <3 0>;
+ touchscreen-size-x = <1024>;
+ touchscreen-size-y = <600>;
+ //touchscreen-swapped-x-y;
+ status = "okay";
+ };
+
+&pinctrl {
+ pinctrl_edt_ft5x06: pinctrl_edt_ft5x06-0 {
+ pins {
+ pinmux = <STM32_PINMUX('B', 3, GPIO)>;
+ };
+ };After modify the devicetree is the following
+&i2c2 {
+ pinctrl-names = "default", "sleep";
+ pinctrl-0 = <&i2c2_pins_a>;
+ pinctrl-1 = <&i2c2_pins_sleep_a>;
+ i2c-scl-rising-time-ns = <185>;
+ i2c-scl-falling-time-ns = <20>;
+ status = "okay";
+ /delete-property/dmas;
+ /delete-property/dma-names;
+
+ polytouch: gt911@5d {
+ compatible = "goodix,gt911";
+ reg = <0x5d>;
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_goodix_gt911>;
+ interrupt-parent = <&gpiob>;
+ interrupts = <3 0>;
+ touchscreen-size-x = <1024>;
+ touchscreen-size-y = <600>;
+ //touchscreen-swapped-x-y;
+ status = "okay";
+ };
+&pinctrl {
+ pinctrl_goodix_gt911: pinctrl_goodix_gt911-0 {
+ pins {
+ pinmux = <STM32_PINMUX('B', 3, GPIO)>;
+ };
+ };The build process finishes without errors but during the boot sequence, the "Kernel panic " message appears and the process stops. Below the consolle log starting from i2c driver loading
[ 2.515121] i2c /dev entries driver
[ 2.536805] stm32f7-i2c 40012000.i2c: can't use DMA
[ 2.541775] stm32f7-i2c 40012000.i2c: STM32F7 I2C-0 bus adapter
[ 2.563780] stm32f7-i2c 40013000.i2c: can't use DMA
[ 2.621395] Goodix-TS 1-005d: ID 911, version: 1060
[ 2.641770] input: Goodix Capacitive TouchScreen as /devices/platform/soc/40013000.i2c/i2c-1/1-005d/input/input0
[ 2.650861] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 2.658434] pgd = (ptrval)
[ 2.661185] [00000000] *pgd=00000000
[ 2.664652] Internal error: Oops: 5 [#1] PREEMPT SMP ARM
[ 2.669905] Modules linked in:
[ 2.672929] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.94 #1
[ 2.678871] Hardware name: STM32 (Device Tree Support)
[ 2.683976] PC is at desc_to_gpio+0x0/0x18
[ 2.688024] LR is at goodix_request_irq+0x14/0x68
[ 2.692672] pc : [<c0716c18>] lr : [<c0c2c3d8>] psr: 60000013
[ 2.698880] sp : db0b5b18 ip : db0c0000 fp : c1964574
[ 2.704055] r10: c144b888 r9 : da04e420 r8 : c1804c48
[ 2.709231] r7 : 00000001 r6 : 00000001 r5 : 00000000 r4 : db4a1dc0
[ 2.715699] r3 : 00002002 r2 : 00000001 r1 : 00000001 r0 : 00000000
[ 2.722171] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 2.729239] Control: 10c5387d Table: c020406a DAC: 00000051
[ 2.734931] Process swapper/0 (pid: 1, stack limit = 0x(ptrval))
[ 2.740882] Stack: (0xdb0b5b18 to 0xdb0b6000)
[ 2.745196] 5b00: db4a1dc0 00000000
[ 2.753306] 5b20: 00000001 00000001 c1804c48 db4a1dc0 00000000 c0c2c81c 00000000 00000000
[ 2.761414] 5b40: db4a1dc0 00000000 da04e400 c0c2cd94 00000000 00000000 00000000 00000000
[ 2.769521] 5b60: 31313939 31390000 10600031 eff0ae88 da04e420 c0c2c9a4 c1963260 da04e400
[ 2.777628] 5b80: 00000000 c1963260 00000000 c0c419ec c19fd2cc da04e420 c19fd2d0 00000000
[ 2.785734] 5ba0: 00000000 c09888a8 da04e420 c1963260 db0b5c24 c0988cc0 00000001 c19fd2a8
[ 2.793841] 5bc0: 00000000 c0988ac8 da04e400 c1963260 da04e420 00000000 c1804c48 db0b5c24
[ 2.801948] 5be0: c0988cc0 00000001 c19fd2a8 00000000 c1964574 c0986c40 c1964574 db20ef6c
[ 2.810055] 5c00: da0259b8 eff0ae88 da04e420 da04e420 c1804c48 da04e454 da01d480 c098863c
[ 2.818161] 5c20: da03ea80 da04e420 00000001 eff0ae88 da04e428 da04e420 c19645a4 da01d480
[ 2.826268] 5c40: da04e420 c0987a50 da04e428 c1804c48 00000000 c0984920 da01d440 00000000
[ 2.834374] 5c60: da04e404 c0994b34 00000000 eff0ae88 da04e420 da04e400 db0b5cc4 da01d440
[ 2.842480] 5c80: 00000000 da04e404 da04e420 c1804c48 da01d440 c0c3ffd4 00000000 c0f26f30
[ 2.850585] 5ca0: 0000005d c1804c48 da01d440 da01d480 dbba2c6c c144e274 da01d480 c0c44794
[ 2.858691] 5cc0: dbba2c98 31397467 00000031 00000000 00000000 00000000 005d0000 00000000
[ 2.866796] 5ce0: 00000000 dbba2c6c 00000000 00000000 00000000 00000000 00000000 eff0ae88
[ 2.874902] 5d00: dbba2c6c dbba2c6c dbba2cbc da01d440 dbba28a0 c0c44ac8 da01d440 00000000
[ 2.883008] 5d20: da01d480 00000000 db0b5dc4 db0b5dc4 c1804c48 c0c40e6c c1203c44 da01d440
[ 2.891115] 5d40: da01d440 00000000 00000000 00000200 db1f3600 db0b5dc4 db0b5dc4 c0c592c0
[ 2.899221] 5d60: 00000000 db2193c0 da01d440 c0f26f84 00000152 db213c80 db1f3610 da03e540
[ 2.907329] 5d80: 000030d4 00002710 00002710 c148734c 006000c0 00000052 40013000 c1965b1c
[ 2.915436] 5da0: da03e540 3b9aca00 51eb851f c1804c48 db1f3600 c1450388 000000b9 00000014
[ 2.923543] 5dc0: 00000000 db0b5dc4 db0b5dc4 eff0ae88 00000001 c1804c48 c1965b30 c0d06484
[ 2.931649] 5de0: 00000000 c04f852c c13c1748 00000000 dbba28a0 c40028e8 c40028e8 c40028e8
[ 2.939755] 5e00: 00000000 eff0ae88 00000000 db1f3610 00000000 c1965b30 00000000 00000000
[ 2.947861] 5e20: c1965b30 00000000 c16cf854 c098a7d0 c19fd2cc db1f3610 c19fd2d0 00000000
[ 2.955968] 5e40: 00000000 c09888a8 db1f3610 c1965b30 db1f3644 c0988bd0 00000000 c16cf834
[ 2.964074] 5e60: c16004a8 c0988ac8 c16cf854 c0f26f30 c1207f80 db1f3610 c1965b30 db1f3644
[ 2.972180] 5e80: c0988bd0 00000000 c16cf834 c16004a8 c16cf854 c0988cbc db213d34 c1804c48
[ 2.980285] 5ea0: c1965b30 c0986b6c c1940c40 db09f458 db213d34 eff0ae88 db09f46c c1965b30
[ 2.988390] 5ec0: da039100 c1940c40 00000000 c0987d10 c14505e0 c1804c48 ffffe000 c1965b30
[ 2.996496] 5ee0: c1804c48 ffffe000 c16a109c c09898e4 c1987120 c1804c48 ffffe000 c0302e5c
[ 3.004602] 5f00: dbfffe36 c0366400 c14d97f8 c1447800 00000000 00000006 00000006 c133e000
[ 3.012709] 5f20: 00000000 c1804c48 c134f1a8 c133e074 c1993e80 dbfffe20 dbfffe28 eff0ae88
[ 3.020815] 5f40: c16cf838 c1987120 c1756788 eff0ae88 c1987120 c1757130 00000007 c1993e80
[ 3.028920] 5f60: c1993e80 c1601128 00000006 00000006 00000000 c16004a8 0000015e 00000000
[ 3.037026] 5f80: db0c8504 00000000 c0f1fe14 00000000 00000000 00000000 00000000 00000000
[ 3.045132] 5fa0: 00000000 c0f1fe1c 00000000 c03010e8 00000000 00000000 00000000 00000000
[ 3.053238] 5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.061344] 5fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 3.069469] [<c0716c18>] (desc_to_gpio) from [<c0c2c3d8>] (goodix_request_irq+0x14/0x68)
[ 3.077479] [<c0c2c3d8>] (goodix_request_irq) from [<c0c2c81c>] (goodix_configure_dev+0x1dc/0x280)
[ 3.086359] [<c0c2c81c>] (goodix_configure_dev) from [<c0c2cd94>] (goodix_ts_probe+0x3f0/0x494)
[ 3.094984] [<c0c2cd94>] (goodix_ts_probe) from [<c0c419ec>] (i2c_device_probe+0x244/0x264)
[ 3.103266] [<c0c419ec>] (i2c_device_probe) from [<c09888a8>] (really_probe+0x1fc/0x2b8)
[ 3.111284] [<c09888a8>] (really_probe) from [<c0988ac8>] (driver_probe_device+0x60/0x168)
[ 3.119474] [<c0988ac8>] (driver_probe_device) from [<c0986c40>] (bus_for_each_drv+0x80/0xc4)
[ 3.127924] [<c0986c40>] (bus_for_each_drv) from [<c098863c>] (__device_attach+0xd0/0x138)
[ 3.136115] [<c098863c>] (__device_attach) from [<c0987a50>] (bus_probe_device+0x84/0x8c)
[ 3.144221] [<c0987a50>] (bus_probe_device) from [<c0984920>] (device_add+0x36c/0x608)
[ 3.152067] [<c0984920>] (device_add) from [<c0c3ffd4>] (i2c_new_device+0x144/0x2d0)
[ 3.159743] [<c0c3ffd4>] (i2c_new_device) from [<c0c44794>] (of_i2c_register_device+0x5c/0x84)
[ 3.168280] [<c0c44794>] (of_i2c_register_device) from [<c0c44ac8>] (of_i2c_register_devices+0x88/0xcc)
[ 3.177592] [<c0c44ac8>] (of_i2c_register_devices) from [<c0c40e6c>] (i2c_register_adapter+0x17c/0x440)
[ 3.186904] [<c0c40e6c>] (i2c_register_adapter) from [<c0c592c0>] (stm32f7_i2c_probe+0xa38/0xe50)
[ 3.195698] [<c0c592c0>] (stm32f7_i2c_probe) from [<c098a7d0>] (platform_drv_probe+0x48/0x98)
[ 3.204146] [<c098a7d0>] (platform_drv_probe) from [<c09888a8>] (really_probe+0x1fc/0x2b8)
[ 3.212338] [<c09888a8>] (really_probe) from [<c0988ac8>] (driver_probe_device+0x60/0x168)
[ 3.220530] [<c0988ac8>] (driver_probe_device) from [<c0988cbc>] (__driver_attach+0xec/0xf0)
[ 3.228894] [<c0988cbc>] (__driver_attach) from [<c0986b6c>] (bus_for_each_dev+0x74/0xb4)
[ 3.237000] [<c0986b6c>] (bus_for_each_dev) from [<c0987d10>] (bus_add_driver+0x1c0/0x204)
[ 3.245192] [<c0987d10>] (bus_add_driver) from [<c09898e4>] (driver_register+0x74/0x108)
[ 3.253215] [<c09898e4>] (driver_register) from [<c0302e5c>] (do_one_initcall+0x54/0x284)
[ 3.261321] [<c0302e5c>] (do_one_initcall) from [<c1601128>] (kernel_init_freeable+0x2d4/0x364)
[ 3.269940] [<c1601128>] (kernel_init_freeable) from [<c0f1fe1c>] (kernel_init+0x8/0x110)
[ 3.278044] [<c0f1fe1c>] (kernel_init) from [<c03010e8>] (ret_from_fork+0x14/0x2c)
[ 3.285539] Exception stack(0xdb0b5fb0 to 0xdb0b5ff8)
[ 3.290544] 5fa0: 00000000 00000000 00000000 00000000
[ 3.298652] 5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.306756] 5fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 3.313313] Code: e30011bd e34c013a ebf0c198 eafffff8 (e5903000)
[ 3.319513] ---[ end trace 9525448ef805ecf3 ]---
[ 3.323969] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 3.323969]
[ 3.332980] CPU1: stopping
[ 3.335647] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G D 4.19.94 #1
[ 3.342968] Hardware name: STM32 (Device Tree Support)
[ 3.348082] [<c031269c>] (unwind_backtrace) from [<c030cd3c>] (show_stack+0x10/0x14)
[ 3.355742] [<c030cd3c>] (show_stack) from [<c0f0b7cc>] (dump_stack+0xb0/0xc4)
[ 3.362898] [<c0f0b7cc>] (dump_stack) from [<c0310b9c>] (handle_IPI+0x418/0x444)
[ 3.370230] [<c0310b9c>] (handle_IPI) from [<c06bbb30>] (gic_handle_irq+0x98/0x9c)
[ 3.377728] [<c06bbb30>] (gic_handle_irq) from [<c0301a0c>] (__irq_svc+0x6c/0xa8)
[ 3.385135] Exception stack(0xdb0eff60 to 0xdb0effa8)
[ 3.390143] ff60: 00000000 00000738 dbb8d54c c031e220 ffffe000 c1804c78 c1804cbc 00000002
[ 3.398247] ff80: c1804c48 00000000 c175f628 c13f0a70 00000000 db0effb0 c0309384 c0309388
[ 3.406348] ffa0: 60000013 ffffffff
[ 3.409808] [<c0301a0c>] (__irq_svc) from [<c0309388>] (arch_cpu_idle+0x38/0x3c)
[ 3.417140] [<c0309388>] (arch_cpu_idle) from [<c0375984>] (do_idle+0x1dc/0x288)
[ 3.424468] [<c0375984>] (do_idle) from [<c0375d08>] (cpu_startup_entry+0x18/0x1c)
[ 3.431966] [<c0375d08>] (cpu_startup_entry) from [<c03025ec>] (__enable_mmu+0x0/0x14)
[ 3.439817] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 3.439817] ]---Why this happens? How to solve it?
Many thanks
Regards