linux-5.4.31 stuck on boot in start_kernel()/arch_cpu_idle()
I'm trying to build linux-5.4.31 for stm32mp1c-ev1 (tag: v5.4-stm32mp-r1). u-boot loads the kernel successfully, but then nothing happens. I've gone in with GDB, and noticed that the kernel is stuck in start_kernel(), and never leaves it.
What is the fix for this?
#0 cpu_v7_do_idle () at arch/arm/mm/proc-v7.S:78
#1 0xc010a1a4 in arch_cpu_idle () at arch/arm/kernel/process.c:71
#2 0xc0158064 in cpuidle_idle_call () at kernel/sched/idle.c:154
#3 do_idle () at kernel/sched/idle.c:263
#4 0xc01583d8 in cpu_startup_entry (state=CPUHP_ONLINE) at kernel/sched/idle.c:355
#5 0xc0acb5b8 in rest_init () at init/main.c:451
#6 0xc0f00a40 in arch_call_rest_init () at init/main.c:573
#7 0xc0f00f10 in start_kernel () at init/main.c:785
#8 0x00000000 in ?? ()