Skip to main content
Associate III
April 27, 2024
Question

Load Bin Using RPROC

  • April 27, 2024
  • 1 reply
  • 805 views

Hello

 

Iam Using Stm32mp157aaa3 processor in my custom board and U boot version 2023.10.Can we load .bin extension file using rproc command in uboot.

 

Tanks & Regards

Srikanth.R

This topic has been closed for replies.

1 reply

Bernard PUEL
Technical Moderator
May 3, 2024

Hello Srikanth,

Yes only ELF format is supported because it contains information about binary location you don't have obviously in the .bin format. 

 

By the way, we support .bin firmware but in this case this is for firmware signed (so for authentication at start up) because this binary is associated with additional tables. But My understanding is not what you want to do (if you are interested, the wiki is describing this more complex use case...). 

 

Also note, on V5 release there was a regression on the feature (M4 load from U-boot). It was solved with this patch: 

https://github.com/STMicroelectronics/linux/commit/89fdf7bece3d1be0d37156897ed8e183d5fcf1e4