LPTIM_TypeDef contains incorrectly sized field uint16_t RESERVED1
The LPTIM_TypeDef struct that is used throughout many of the HAL header files contains a few RESERVED fields that cover unused address offsets in the peripheral's memory map.
The first of these, RESERVED1, is declared as uint16_t. I believe that this is incorrect and that it should be a uint32_t field to ensure that the address offsets of the subsequent fields are correct.

Could someone please double-check and correct this if necessary?