Op-tee Debug message: print_probe_list:409 Failed list: 0 elements
It's fun to debugging the output when I flashing the processor/eMMC from CubeProgrammer via USB. But it's less fun to not knowing the cause of the error.
What can it be in this case?
Do I have forgot the sett the board ID, is the unknown VDD the error?
What I have done, is to copy the most of stm32mp15xx-dk1.dtsi into stm32mp15x-<your project device tree>-mx.dts because my custom made bord is the same as STM32MP157D-DK1 + eMMC boot.
See the post here: Debug Output UART
My device tree .dts files: Device Tree STM32MP151AAC3