SDMMC2 HAL SDIO write multiple blocks (SDIO CMD53) issue
Good morning,
I am trying to send a buffer consisting of 896 elements to a Wi-Fi Chip from STM32MP131. I am trying to use the HAL Driver DMA (which uses interrupt to transfer blocks using IDMA).
Although the code has several checks and balances. I am not encountering any failure when that function is processed. I monitored with the logic analyzer, and I am seeing transmission. But I suspect that the transmission did not go through well. I tried to read the set of values with and without writing and the values are same Indicating that the receiver has not responded.
If I use polling instead of IDMA. the receive FIFO is empty when trying to receive. I cannot send through polling and receive through interrupt as that would be an interrupt issue.
I tried to send the set of elements byte by byte using CMD52. In that case the tests are failing.
Kindly suggest and help me here. If possible, point me to a location where I have access to some HAL_SDIO drivers that can be used for STM32MP131.
Thanks and best regards
Sricharan Kidambi S