Secure boot: mutable extlinux.conf in bootfs during updates allows boot flow manipulation - recommended solution?
Description
Hello,
we are currently integrating secure boot on an STM32MP15-based platform using the ST OpenSTLinux ecosystem (TF-A + OP-TEE + U-Boot + RAUC / ST update solution here: https://github.com/STMicroelectronics/meta-st-ota/).
During this work, we identified a potential gap in the chain of trust related to the boot filesystem (bootfs), specifically the use of a mutable extlinux.conf.
Problem
In our current setup:
- TF-A authenticates FIP (OP-TEE + U-Boot)
- U-Boot supports FIT signature verification for kernel / DTB / initramfs
- extlinux.conf is stored in bootfs (ext4) and remains writable - this post-install.sh changes rootfs partuuid after each update.
- U-Boot uses extlinux.conf to select kernel / DTB and to define kernel command line (`root=PARTUUID=e91c4e10...`). This PARTUUID is changed after the update.
With secure boot enabled, if extlinux remains mutable, it cannot be signature-protected, which violates the chain of trust.
Question
What is the recommended approach in ST architecture to handle this?
Specifically:
- Is there an ST-recommended way to protect or authenticate extlinux.conf?
- Are there existing patches for this problem?
Any guidance, best practices, or references to ST-secured designs would be highly appreciated.
Thanks in advance!